---
title: "Alphabet Soup Part II: Swagelok Acronyms From F to N"
description: Here are some acronyms you may have run into on our site, and what all those letters mean from F to N.
---

<https://edmontonsolutions.swagelok.com/blog>

# [Alphabet Soup Part II: Swagelok Acronyms From F to N](https://edmontonsolutions.swagelok.com/blog/alphabet-soup-part-ii-swagelok-acronyms-from-f-to-n)

 Written by [Katie Reid](https://edmontonsolutions.swagelok.com/blog/author/katie-reid) | Fri, Oct 16, 2015 @ 22:10 PM

#### There are some long and informative names behind all those letter combinations

<https://edmontonsolutions.swagelok.com/blog>

*Product groupings that have common Swagelok acronyms include the [Pre-Engineered Subsystem](http://edmontonvalve.swagelok.com/blog/bid/228828/Webinar-Gives-Detailed-Look-at-Swagelok-Pre-Engineered-SubSystems) products, [regulator series](http://edmontonvalve.swagelok.com/blog/bid/357116/two-ways-to-find-the-right-size-pressure-regulator-for-the-job), and Swagelok fittings.*

In an [earlier post](http://edmontonvalve.swagelok.com/blog/Alphabet-Soup-A-E-Shedding-Some-Light-On-Swagelok-Acronyms) we went through some of the acronyms you'll run into when you read our blog. Last time we covered letters A through E. This time we continue on through the middle of the alphabet. Check back to see future posts that will take us all the way to Z.

**FDH** – [**F**luid **d**istribution **h**eaders](http://edmontonvalve.swagelok.com/free-fluid-distribution-header-catalogue) are common components used in a variety of gas and liquid applications. An FDH provides a flow path while allowing multiple outlets, acting much like a large branch fitting. This is one of the many preassembled subsystems available from Edmonton Valve & Fitting.

**FLIR **– **F**orward **l**ooking **i**nfrared **r**adiometer cameras are sophisticated thermal-imaging tools for detecting leaks. Any time there's a problem that generates heat, a [FLIR camera](http://edmontonvalve.swagelok.com/blog/bid/313373/Swagelok-Leak-Detection-FLIR-Cameras-for-Hire) can find it. A hydrocarbon leak shows up as a cloud on the camera screen, even though it's invisible to the naked eye.

**FLM** – [**F**ast **l**oop **m**odules](http://edmontonvalve.swagelok.com/fast-loop-module-catalogue) are designed to handle high flows in sample transport lines to reduce time delays for online analyzer systems. Located at the analyzer shelter and offering a bypass, the Swagelok FLM can isolate the sample system and introduce a purge gas for system cleaning. The FLM extracts a sample through a filter while using the high flow rate of bypass to keep the filter element clean. 

**FSM **– When analyzing a gas sample, it's important to move the sample quickly. One way to speed up delivery is to lower the pressure. That's where a Swagelok **f**ield **s**tation **m**odule comes in. When this pre-engineered subassembly is placed directly off the supply tap, it lowers the pressure of a gas as soon as possible.

**ISO **– The **I**nternational **O**rganization for **S**tandardization is an independent, non-governmental membership organization that sets standards of all kinds, from standard musical pitch (ISO 16) to sample preparation of iron ore (ISO 3082) to software testing (ISO 29119). Edmonton Valve & Fitting supports and maintains the ISO 9001 standard for quality management systems.

**K Series** – The letter K in our K Series regulators is a nod to the series origins at **Kenmac** Ltd., a British company that Swagelok acquired back in 2003. At the time, regulators were the only gap in Swagelok’s product line for analytical instrumentation. Since then, Swagelok has closed the gap to become your supplier for sample handling. The K Series includes 17 different models of pressure-reducing, backpressure and specialty regulators.

**MPC **– Our [**M**odular **P**latform **C**omponent](http://edmontonvalve.swagelok.com/mpc-catalogue) system lets you pack more instrumentation into less space. A substrate channel holds the drop-in components that provide the main flow path. Then it's literally a snap to add surface-mount components to create the fluid distribution system. Swagelok also makes an interactive software tool called the MPC Configurator to help you plan out the details.

**MTR** – When a customer purchases tubing, they are able to conveniently access our [**m**aterial **t**est **r**eport](http://edmontonvalve.swagelok.com/blog/bid/357089/Need-Tubing-Material-Test-Reports-Edmonton-Valve-Has-Them-Online) website that will provide details on tubing heat numbers. For example, a sheet might tell you that a particular type of welded tubing contains so much chromium, nickel, and other elements. It also could list the tensile strength, hardness, and other properties. It also show that the product has passed a series of tests. 

**NPT **– The **N**ational **P**ipe **T**hread standard applies to tapered threads on [pipes and fittings](http://edmontonvalve.swagelok.com/blog/bid/357189/Swagelok-Tube-Fitting-Advantage-Still-Strong-after-67-Years). NPT threads usually require application of sealing compound or tape to prevent leaks.

Up next we will be posting acronymns in the **P-R** range! 

**Additional resources**

- **[5 Tips for Tubing Installation from Swagelok](http://edmontonvalve.swagelok.com/blog/bid/351205/5-Tips-for-Tubing-Installation-from-Swagelok)**
- **[4 Solutions from the Swagelok Tube Adapter](http://edmontonvalve.swagelok.com/blog/bid/340772/4-Solutions-from-the-Swagelok-Tube-Adapter)**
- **[Preventing Creep in Pressure Regulators](http://edmontonvalve.swagelok.com/blog/bid/303179/Preventing-Creep-in-Pressure-Regulators)**

In a hurry or have a question? [Please click here to get in touch - we respond fast!](https://edmontonsolutions.swagelok.com/ask) Or call 780.437.0640.

 

[View full post](https://edmontonsolutions.swagelok.com/blog/alphabet-soup-part-ii-swagelok-acronyms-from-f-to-n)

```json
{
  "@context" : "http://schema.org",
  "@type" : "BlogPosting",
  "author" : {
    "@type" : "Person",
    "name" : "Katie Reid"
  },
  "dateModified" : "2017-03-23T14:47:14.143Z",
  "datePublished" : "2015-10-16T22:00:00Z",
  "headline" : "Alphabet Soup Part II: Swagelok Acronyms From F to N",
  "image" : {
    "@type" : "ImageObject",
    "height" : 336,
    "url" : "http://edmontonvalve.swagelok.com/hubfs/acronyms_F-N.png",
    "width" : 345
  },
  "mainEntityOfPage" : "https://edmontonsolutions.swagelok.com/blog/alphabet-soup-part-ii-swagelok-acronyms-from-f-to-n",
  "publisher" : {
    "@type" : "Organization",
    "logo" : {
      "@type" : "ImageObject",
      "height" : 60.0,
      "url" : "https://www.edmonton.swagelok.solutions/hubfs/23%20Logos/Swagelok%20Edmonton%20Logo%202024%20400x200.webp",
      "width" : 120.00001
    },
    "name" : "Industrial Fluid Systems Blog"
  }
}
```