---
title: 5 Facts About Swagelok Gauges
description: Make sure you're using gauges correctly -- learn the 5 Laws Of Swagelok Gauges.
---

<https://edmontonsolutions.swagelok.com/blog>

# [5 Facts About Swagelok Gauges](https://edmontonsolutions.swagelok.com/blog/bid/335790/5-facts-about-swagelok-gauges)

 Written by [Taryn Hardes](https://edmontonsolutions.swagelok.com/blog/author/taryn-hardes) | Wed, Mar 05, 2014 @ 21:03 PM

***We already gave you the [five laws of gauge installation](https://edmontonsolutions.swagelok.com/blog/bid/310502/The-Five-Laws-Of-Swagelok-Gauges) - now we have five facts about the gauges themselves.***

## **1. Most gauges mechanically measure pressure using a bourdon tube**

A bourdon tube works as a sensing element. Bourdon tubes, which are commonly found in Swagelok gauges, work like a party horn. It will try to flatten itself with an increase in pressure, which pulls up on the lever which pulls the dial to show the appropriate pressure reading. A decrease in pressure allows the bourdon tube to return to its original C shape. Another option is a diaphragm, which are typically used for lower pressures gauges such as the L Model.

## **2. You’ll get your most accurate reading in the middle third of the dial**** **

|  |   |
| --- | --- |

 

When choosing the right gauge for a job, be sure to select a range that allows your normal system to fall in the centre of the dial. For example, if your system pressure is 100 psi, consider using a 200 psi gauge.

 

## **3. Bigger dials are more accurate** 

Some Swagelok gauges are available in a variety of face diameters. Normally the larger the dial diameter, the more accurate the reading. Try to use as large of a face as you can in highly sensitive applications.

## **4. There are three mount configuration options for your convenience**

****

Swagelok gauges comes in a lower back mount, centre back mount, and lower mount for your convenience. Lower mount is most common, available on every Swagelok gauges series.

## **5. Gauges can come with a Tube Adapter end connection to allow for ideal alignment**** **

|  |   |
| --- | --- |

Many gauge designs utilize pipe fittings to connect the gauge into a system. This can create alignment issues and can even risk leaks by NPT threads being over or under tightened. Swagelok Pressure Gauges offer a unique end connection option that simplifies installation – the Swagelok Tube Adapter.

Swagelok Tube Adapter end connections eliminate alignment problems because the gauge dial can be aligned to the desired position and then remain stationary during pull-up of the fitting.

To learn more about the pressure gauge products available from Swagelok, [download the Pressure Gauge catalogue](https://edmontonsolutions.swagelok.com/measurement).

 

 

[View full post](https://edmontonsolutions.swagelok.com/blog/bid/335790/5-facts-about-swagelok-gauges)

```json
{
  "@context" : "http://schema.org",
  "@type" : "BlogPosting",
  "author" : {
    "@type" : "Person",
    "name" : "Taryn Hardes"
  },
  "dateModified" : "2021-05-20T17:20:52.585Z",
  "datePublished" : "2014-03-05T21:20:00Z",
  "headline" : "5 Facts About Swagelok Gauges",
  "image" : {
    "@type" : "ImageObject",
    "height" : 174,
    "url" : "//cdn2.hubspot.net/hub/165880/file-521577627-png/images/gauge_sweet_spot.png",
    "width" : 176
  },
  "mainEntityOfPage" : "https://edmontonsolutions.swagelok.com/blog/bid/335790/5-facts-about-swagelok-gauges",
  "publisher" : {
    "@type" : "Organization",
    "logo" : {
      "@type" : "ImageObject",
      "height" : 60.0,
      "url" : "https://www.edmonton.swagelok.solutions/hubfs/23%20Logos/Swagelok%20Edmonton%20Logo%202024%20400x200.webp",
      "width" : 120.00001
    },
    "name" : "Industrial Fluid Systems Blog"
  }
}
```