---
title: Fluid Distribution Headers Save Space And Time
description: Fluid Distribution Headers are one of the many preassembled subsystems available from Edmonton Valve & Fitting used in a variety of gas and liquid applications.
---

<https://edmontonsolutions.swagelok.com/blog>

# [Fluid Distribution Headers Save Space And Time](https://edmontonsolutions.swagelok.com/blog/fluid-distribution-headers-save-space-and-time)

 Written by [Alecia Robinson](https://edmontonsolutions.swagelok.com/blog/author/alecia-robinson) | Wed, May 03, 2017 @ 20:05 PM

#### Get the configuration you want and get it quickly from Edmonton Valve & Fitting

<https://edmontonsolutions.swagelok.com/free-fluid-distribution-header-catalogue>

***F**luid **D**istribution **H**eaders are common components used in a variety of gas and liquid applications. Download a free copy of the the [FDH catalogue](https://edmontonsolutions.swagelok.com/free-fluid-distribution-header-catalogue) one of the many preassembled subsystems available from Edmonton Valve & Fitting. *

When you have multiple fluid lines serving the same purpose, a fluid distribution header can be a great way to organize everything and save space. It has an inlet on one end, a drain on the other end, and multiple outlets on the sides. Typically, it has a main isolation valve and several outlets, each with its own isolation valve. For potentially wet gases, such as compressed air or steam, the header can be installed vertically with a drain valve at the bottom.  For liquid service, install it vertically, with the supply entering at the bottom and the top valve acting as a vent for removing trapped air or allowing air in for draining during maintenance.

Maybe you have a cleaning station where you need to handle a half-dozen cylinders at the same time. Maybe you need an instrument air header, or an LP steam header. Consider it any time you have multiple runs coming off the same input. Run the fluid in the opposite direction, and a fluid distribution header can serve as a collection manifold.

Two mounting brackets allow you to mount the header on an aluminum plate, a steel stand, or a piece of pipe.

### Space and time

The compact design is only one advantage over trying to accomplish the same job with pipe or tubing and separate components. It also has fewer connection points, meaning less opportunity for a leak to appear.

Ordering a fluid distribution header from Edmonton Valve & Fitting also saves you a day of work putting all the parts together. Because we assemble fluid system components all the time, we have the tools and the expertise to do it right. We also test every fluid distribution header that we make with nitrogen at 250 psi, plus liquid leak detector. We can do hydro testing up to 1,000 psi if you like.

And the entire assembly comes under a single part number, making it easy to order.

### Locally made

Swagelok's fluid distribution headers are available in 1-inch and 2-inch sizes. The 1-inch platform is good for working pressures up to 3,000 psi, while the 2-inch platform can handle up to 1,000 psi. The extruded manifold body design features squared sides that mount solidly and prevent twisting. It can be ordered with 2 to 16 branch outlets, with or without valves, so you can add ports as needed without welding.

You get two more advantages when you order a fluid distribution header from Edmonton Valve and fitting. First, we're happy to customize it for your particular needs. For instance, you can order the header with instrumentation ball valves, process ball valves, integral bonnet needle valves or plug valves. We can put the outlets all on one side, if you like, and fit it with a variety of connection types. We can join two headers to handle 18 lines.

The second advantage is that, because we assemble them right here in Edmonton, you can get them quickly. If you chose a standard configuration, we can turn it around in a few days. Tell us the details of what you need [through our website](http://edmontonvalve.swagelok.com/ask?__hssc) or by calling 780-437-0640.

**Additional resources**

-  **[Freezing Weather's Almost Gone, But It's Not Forgotten](http://edmontonvalve.swagelok.com/blog/freezing-weathers-almost-gone-but-its-not-forgotten)**
- **[Customers Asked, Edmonton Valve Responded: the Steam Lance](http://edmontonvalve.swagelok.com/blog/customers-asked-edmonton-valve-responded-the-steam-lance)**
- **[Edmonton Valve’s CNC Bender Makes Quick Work of Custom Orders](http://edmontonvalve.swagelok.com/blog/edmonton-valves-cnc-bender-makes-quick-work-of-custom-orders)**

[View full post](https://edmontonsolutions.swagelok.com/blog/fluid-distribution-headers-save-space-and-time)

```json
{
  "@context" : "http://schema.org",
  "@type" : "BlogPosting",
  "author" : {
    "@type" : "Person",
    "name" : "Alecia Robinson"
  },
  "dateModified" : "2017-05-02T15:42:56.080Z",
  "datePublished" : "2017-05-03T20:00:00Z",
  "headline" : "Fluid Distribution Headers Save Space And Time",
  "image" : {
    "@type" : "ImageObject",
    "height" : 298,
    "url" : "http://edmontonvalve.swagelok.com/hs-fs/hub/165880/file-1145985356-png/FDH.png",
    "width" : 495
  },
  "mainEntityOfPage" : "https://edmontonsolutions.swagelok.com/blog/fluid-distribution-headers-save-space-and-time",