---
title: "Swagelok Valve for Chlorine Service: Ball Vent and Carbon Steel Body"
description: Our Chlorine Series valves maximize safety and reliability, meeting strict industry standards. Learn about their precision engineering & download details.
---

<https://edmontonsolutions.swagelok.com/blog>

# [Swagelok Valve for Chlorine Service: Ball Vent and Carbon Steel Body](https://edmontonsolutions.swagelok.com/blog/swagelok-valve-for-chlorine-service-ball-vent-and-carbon-steel-body)

 Written by [James Dickie](https://edmontonsolutions.swagelok.com/blog/author/james-dickie) | Tue, Apr 09, 2024 @ 13:04 PM

Swagelok's C60V Series valves, designed for chlorine applications, combine carbon steel bodies with virgin PTFE seats for optimal safety and adherence to Chlorine Institute guidelines. These valves feature a ball vent to prevent overpressurization, undergo rigorous testing for reliability, and are meticulously cleaned and packaged for immediate chlorine service use.

Swagelok's Chlorine Series (C60V Series) valves are designed with specific materials to ensure safety and reliability when handling chlorine applications. The valve body is made of carbon steel, paired with virgin PTFE seats and packing.

<https://www.edmonton.swagelok.solutions/products/valves>

This construction adheres to the stringent guidelines in Chlorine Institute Pamphlet 6, which covers Piping Systems for Dry Chlorine, ensuring compatibility and safety in chlorine service environments.

These valves also feature an upstream ball vent that prevents overpressurization in the ball and body when the valve is closed, further enhancing operational safety and reliability. C60V valves offer pressure-temperature ratings of 300 psig at temperatures ranging from –20 to 250°F (20.6 bar at –28 to 121°C), good for a range of chlorine service applications.

## <https://edmontonsolutions.swagelok.com/hs/cta/wi/redirect?encryptedPayload=AVxigLLHee7QMPQ%2BH68g0APnY%2BYY%2Bz1iLj%2BeLYEUPMhHdE9JzCa8iKhBKXKfN3Vv8OcoU1aPIfyannqwVedVT0GDwe8BiX0jQzdzD7Jtvb2UNPAx1Ev1z%2Fi4uA4u0c%2BNlkR6KrlO0HBOxAoiLx47pHyEQGHFe7BcNVJvaiIq2Eu1zkt7vLf1g9Si6Iv4VdnoioWTT3xZ5fgUtSdNLFc%3D&webInteractiveContentId=152011585454&portalId=165880> Readiness for immediate use

For cleanliness and safety, the valve bodies and flanges undergo a two-step cleaning process:

- First, with mineral spirits
- Second, with aqueous cleaning solution containing a surfactant

(All other wetted components are cleaned according to Swagelok's Special Cleaning and Packaging SC-11 standards.)

## Capped, sealed, and tagged

To ensure their integrity and readiness for chlorine service, C60V series ball valves are individually capped and sealed in desiccant packaging. And each valve is tagged for chlorine service, emphasizing its specialized use.

Moreover, every valve within the chlorine series undergoes rigorous factory testing, including both seat and shell tests with nitrogen at 300 psig (20.6 bar). These tests are stringent, with seats having a maximum allowable leak rate of 0.04 std cm^3/min, ensuring the valves meet high standards of quality and reliability for handling chlorine.

## Special alloys

Swagelok carries an array of special alloys to meet our customer's requirements. Two important pieces to note:

- Alloy 600, a nickel-chromium-iron alloy. This strong alloy is highly resistant to chloride-ion induced stress corrosion cracking.
- Titanium alloys. They have excellent resistance to corrosion in a wide variety of environments including seawater, salt brines, inorganic salts, bleaches, wet chlorine, alkaline solutions, oxidizing acids and organic acids.

There is often an elevated chlorine level in boiler water, for example. Chlorine and stainless steels don’t mix well and it is common to find stress corrosion cracking in applications that have high chloride levels and stainless steel fittings and tubing. Again, there are a number of materials that we offer that can provide the necessary corrosion resistance in this type of application.

## Chlorine applications support

Swagelok Edmonton offers [certified fluid system experts](https://edmontonsolutions.swagelok.com/blog/what-to-expect-when-a-swagelok-field-advisor-visits) who help customers take action on fluid system challenges. Talk with our team about instrumentation, leaks, seal flush plans, and more. Combine, adapt, and/or tailor services so you get the advice you need. Choose onsite or virtual collaboration.

## Download 60 Series Ball Valve catalogues and more

Get literature on 60 Series, One-Piece Instrumentation, and several other valve lines.

## Getting help with valves

Requesting evaluation and advice from a Swagelok Edmonton Field Advisor is a great way to start any project involving fluid systems. We listen to understand your priorities, gather information on your systems and routines, conduct onsite inspections as appropriate, and offer detailed recommendations. Our goal is to help identify opportunities to increase reliability while lowering your operating costs and minimizing risks. Both onsite and remote support are available. [More →](https://edmontonsolutions.swagelok.com/services/field-advisory)

## Related articles

- <https://www.edmonton.swagelok.solutions/blog/choosing-swagelok-tubing-and-fitting-alloys-use-engineered-combinations-to-resist-corrosion-minimize-cost-pdf-new-video>[High-Pressure Corrosive Environment? High-Temperature Vacuum Environment? Meet Our FX Series Metal Hose (Video, Cutaway)](https://www.edmonton.swagelok.solutions/blog/high-pressure-high-temp-and-or-highly-corrosive-environment-consider-our-fx-series-metal-hose-video-cutaway)
- [Choosing Swagelok Tubing & Fitting Alloys? Engineered Combinations Resist Corrosion & Minimize Cost](https://www.edmonton.swagelok.solutions/blog/choosing-swagelok-tubing-and-fitting-alloys-use-engineered-combinations-to-resist-corrosion-minimize-cost-pdf-new-video)
- [Replacing Industrial Valves? Use This 7-Step Method to Verify Selection](https://www.edmonton.swagelok.solutions/blog/replacing-industrial-valves-use-this-7-step-method-to-verify-selection)
- [FAQ: Which is the Correct 60 Series Ball Valve?](https://www.edmonton.swagelok.solutions/blog/faq-which-is-the-correct-60-series-ball-valve)
- [Bend Your Emissions Curve with Swagelok Low-E Valves (New Video, Free PDF)](https://www.edmonton.swagelok.solutions/blog/bend-your-emissions-curve-with-swagelok-low-e-valves-new-video)

[View full post](https://edmontonsolutions.swagelok.com/blog/swagelok-valve-for-chlorine-service-ball-vent-and-carbon-steel-body)

```json
{
  "@context" : "http://schema.org",
  "@type" : "BlogPosting",
  "author" : {
    "@type" : "Person",
    "name" : "James Dickie"
  },
  "dateModified" : "2024-08-07T22:30:29.589Z",
  "datePublished" : "2024-04-09T13:45:00Z",
  "headline" : "Swagelok Valve for Chlorine Service: Ball Vent and Carbon Steel Body",
  "image" : {
    "@type" : "ImageObject",
    "height" : 467,
    "url" : "https://www.edmonton.swagelok.solutions/hubfs/000%202023/Featured/Special%20Application%20Ball%20Valves%20--%20Chlorine%20Series.webp",
    "width" : 700
  },
  "mainEntityOfPage" : "https://edmontonsolutions.swagelok.com/blog/swagelok-valve-for-chlorine-service-ball-vent-and-carbon-steel-body",