---
title: How to Reduce Fugitive Emissions in Edmonton Refineries
description: Fugitive emissions in a refinery can lead to operator hazards, regulatory correction, and inefficiency. LDAR, as well as certain likely emitters, are examined.
---

[780-437-0640](tel:780-437-0640)           [Locations](https://edmontonvalve.swagelok.com/ask)           [News](https://edmontonvalve.swagelok.com/blog)           [Covid](https://edmontonvalve.swagelok.com/covid19)           [Login](https://products.swagelok.com/en/login)

[![Swagelok Edmonton homepage](https://edmontonvalve.swagelok.com/hubfs/000%202023/Headers/2023%20logo%20WHT%20p0.webp "Swagelok Edmonton homepage")](https://edmontonsolutions.swagelok.com/?hsLang=en)

Search

**Menu**

** **

[![COVID](https://no-cache.hubspot.com/cta/default/165880/608cd187-e808-4e7b-8bea-28d8f4c54c89.png)](https://cta-redirect.hubspot.com/cta/redirect/165880/608cd187-e808-4e7b-8bea-28d8f4c54c89)

[![SHOP](https://no-cache.hubspot.com/cta/default/165880/928cd817-843f-41d0-bc9a-b50fcb5e32db.png)](https://cta-redirect.hubspot.com/cta/redirect/165880/928cd817-843f-41d0-bc9a-b50fcb5e32db)

# How to Reduce Fugitive Emissions in Edmonton Refineries

Leak detection and repair form the backbone of reducing fugitive emissions in a refinery.

![edmonton-reduce-fugitive-emissions-refineries](https://edmontonvalve.swagelok.com/hubfs/edmonton-reduce-fugitive-emissions-refineries.jpg)From start to finish, fugitive emissions are a stumbling block for a refinery. Inefficient at best and hazardous at worst, facilities need to provide a clear outline to operators on how to correct these leaks when they arise. At the heart of any successful campaign is leak detection and repair, known shorthand as LDAR. 

LDAR aims to catch and alleviate current leaks, but also expand its scope to monitor when and why leaks may be occurring. To best understand how to curb fugitive emissions of a refinery, the flow of the LDAR system is key. Additionally, with a general overview of LDAR functions, the system can be better adjusted to the needs of its users. With a proper LDAR system implemented, the focus can turn to some of the more notorious elements for fugitive emissions in a fluid system and how best to maximize their functionality while [minimizing the occurrence of fugitive emissions](https://edmontonvalve.swagelok.com/blog/fugitive-emissions-plan-edv).

## How Does Leak Detection and Repair Reduce Fugitive Emissions in a Refinery?

When discussing LDAR, it’s important to note that the issue of leaks is not as simple as a search and rectification; LDAR is an iterative process of remedying active leaks while [preventing future emission events](https://edmontonvalve.swagelok.com/blog/fugitive-emission-leak-detection-edv). Here’s a look at what an LDAR system may broadly entail:

### Component Identification

To help make the logistics of tracking thousands of possible emission points easier, each component should be provided with a unique identifier. All relevant documentation, and especially diagrams indicating the physical location within the fluid system, should include this identifier. If possible, components can be tagged or otherwise demarcated. Maintenance logs should include the identifier of a component as well as identifiers of any successive replacements in the same location. Not only will tracking identifiers in this manner help quality assurance and control account for the service life of devices, but it can also be of use to diagnose underlying points of the system causing more rapid degradation of components than is to be expected.

### Setting a Minimum Leak Threshold

There are two approaches to consider: setting a universal threshold according to the most exacting leakage rate, or allowing the component specifications to dictate their own leakage rates. This is a bit of an oversimplification as local and federal regulation will also play a role in shaping emission guidelines. Assuming that priority is met, the design of the leak detection threshold weighs ease of tracking versus ease of implementation. Additionally, a universal threshold designed to the lowest (or lowest reasonable) leakage rate across the fluid system may prove costlier at component point-of-purchase and maintenance, but also ensures the greatest retention of products and fewest emissions. However, it is also possible that the system constraints such as temperature and pressure may override some low-emission component designs.

### Observations

The observational period and the effectiveness of measurement tools will be the most important diagnostic step in an LDAR system. Tools must be calibrated and tested for accuracy during field use. Operators need also be trained for the reliability of testing (duration of data collection, distance to measure from source, etc.) to promote measurement confidence. Electronic logging of data can help to cut down on reading and writing reporting errors.

### Maintenance 

Once a leak is detected, repairs need to be performed in a timely manner to reduce fugitive emissions. While still observing the component or components in question, maintenance work in the immediate vicinity, such as tightening of bolts or stem packing materials, or lubricating, will be the first line of defense as it may correct the issue without causing downtime or the need for a part replacement. Failing that, the component should be assessed to determine if its replacement would require a partial or full system shutdown. The part can only be considered repaired once the component or replacement component is measured to leak below the established threshold.

### Maintaining Data Logs

Keeping detailed information of leakage rates, incidence, repair dates, etc. provides a facility with hard data, useful for self-analysis or auditing. From an internal perspective, an operation can hone in on problematic sections of its design in the pursuit of greater efficiency. 

With a more concrete concept of the LDAR process, some common emission vectors in a refinery include valves, flanges, and threaded fittings. Each is analyzed in more detail below.

## Fugitive Emissions Largely Stem from Valves

Valves represent the [greatest source of fugitive emissions](https://edmontonvalve.swagelok.com/blog/fugitive-emissions-ball-valve-canadian-plants-edv) throughout a refinery. This is in part due to the pervasiveness of valves throughout a fluid system as well as limitations inherent to their design. The valve stem provides an avenue for fluid leakage when the packing fails or is not designed to account for low-emission installations. For quarter-turn valves, API 641 sets a maximum allowable leakage rate of 100 ppm by volume during a series of tests meant to simulate both operable temperature extremes as well as a modest amount of open-close cycles. 

Swagelok ball valves offer both single-piece encapsulated packing and capsule seat packing across the appropriate product lines. While the single-piece encapsulated packing has been designed to further reduce leak points, both packings are eligible for API 641 low emission certification.

## The Many Faces of Flanges

![edmonton-faces-flanges-1](https://edmontonvalve.swagelok.com/hubfs/edmonton-faces-flanges-1.png)

Flanges function as an interface between piping and tubing systems, and as such, need to provide an effective seal to prevent fugitive emissions. Some considerations for what goes into establishing an effective and long-lasting seal include:

- **One-piece body: **A seemingly simple but crucial element of design. The fewer individual pieces that compose a greater assembly, the fewer material discontinuities that could leak or develop cracks due to wear. 
- **Material: **Different process fluids require a material that is well-suited for its intrinsic proprieties. Failure to address temperature, pressure, corrosivity, or the ability to embrittle could lead to rapid breakdown of the flange material, potentially in a catastrophic manner.
- **Flange face:** The size of the flange face will constrain the material of the gasket; note that if: 

| P= | F |
| --- | --- |
| A |  |

(where P is pressure, F is force, and A is area), a decrease in surface area means a greater pressure for the same fluid force. A smaller flange face must therefore contain a gasket of harder material to withstand the increase in pressure. Flange faces can come in a variety of styles; some of the most common ones are outlined below:

- **Flat face:** The seal performs best in relatively low temperature and pressure system processes, utilizing a soft gasket that spans the length from inner to outer flange diameter. The large sealing area offers resistance to some forms of mechanical failure.
- **Raised face:** Similar in many ways to the flat face, the raised mating face protrudes outwards from the plane where the bolts are driven through to secure the joint. As such, the seal only runs from the inner diameter to the edge of the mating face. The raised face is extremely prominent in refineries and possesses superior temperature and pressure capabilities compared to the flat face design.
- **Ring-type joint (RTJ):** For extreme temperature and pressure requirements, the RTJ is an option. The gasket of the RTJ is of a much harder metallic material than the semi-metallics often found in a raised face. The gasket will sit in-between the grooved portion of a flange and inhibit direct contact in the joint.

Swagelok flanges meet different regional standards, such as ASME, DIN, and EN, and additional requirements such as API standards are also available. 

## Compression Fittings Inhibit Fugitive Emissions

There are many types of threaded fittings, but some are more susceptible to fugitive emissions than others. Although it is not a universal option, compression fittings are an excellent choice when available to curtail emissions. Where appropriate, compression will offer superior protection against leakage; this property arises from the interaction of the front and back ferrule. When placing the fitting on the tube, the front ferrule seals against the fitting itself, while the back ferrule seals against the tubing, offering an excellent grip of the tube to aid in vibration resistance. A larger surface area of the back ferrule where it contacts the tubing also prevents crimping and puncture.

## Edmonton Valve & Fitting: Committed to Fighting Fugitive Emissions

Fugitive emissions of a refinery are a nuisance on multiple levels. They reduce your plant’s efficiency while posing a threat to your operators at appreciable levels. There are only savings and peace of mind to be gained by reducing fugitive emissions to the lowest possible levels. Beyond those concerns, there are ever-looming regulatory fines and penalties for refineries that are unsuccessful in their attempts to curb emissions as Edmonton and the rest of Canada marches to the goal of a 40-45% reduction of 2012 fugitive emission levels by 2025. 

For all the complexities of your fluid system and the value of its uninterrupted uptime, let an Edmonton Valve & Fitting [Field Advisor](https://edmontonvalve.swagelok.com/field-advisory-services-edv) collaborate on your system design to offer top-notch performance and reliability. Combatting fugitive emissions in your facility may seem dizzying, but our experts can provide you with exceptional support and operator training to assist your efforts every step of the way.

**To find out more about how [Edmonton Valve & Fitting](https://edmontonvalve.swagelok.com/) can curb emissions and increase efficiency, contact us[through our website](https://edmontonvalve.swagelok.com/ask) or by calling 780-437-0640.**

![edmonton-fugitive-emissions-plan-link](https://edmontonvalve.swagelok.com/hubfs/edmonton-fugitive-emissions-plan-link.jpeg)

**

#### Fugitive Emissions Plan

Learn more about fugitive emissions, the root causes, and how to mitigate them.

**More →**

<https://edmontonvalve.swagelok.com/fugitive-emissions-alberta-edv>

![](https://edmontonvalve.swagelok.com/hubfs/iStock-866120916-1.png)

**

#### Field Advisory Services

Learn more about Field Advisory team and how they can help ensure the success of your pipelines. 

**More →**

<https://edmontonvalve.swagelok.com/field-advisory-services-edv>

![](https://edmontonvalve.swagelok.com/hubfs/locations-1.png)

**

#### View Locations

We serve northern and central Alberta from offices in Edmonton, Drayton Valley, and Fort McMurray.

**More →**

<https://edmontonsolutions.swagelok.com/locations?hsLang=en>

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

![](https://cdn2.hubspot.net/hubfs/273774/mp/themes/Act-Theme/images/act-content-card-banner.jpg)

**

#### Get Started With Cards

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Suspendisse tempor nisi ut vehicula commodo.

[Learn More →](https://edmontonsolutions.swagelok.com/fugitive-emissions-refinery-edv#)

### How can we help you today?

Whether you need a single component or help with complex systems, we are here to help.

[![Get in touch](https://no-cache.hubspot.com/cta/default/165880/caa25e34-7e4d-43a5-b37e-96f8be1ab1af.png)](https://cta-redirect.hubspot.com/cta/redirect/165880/caa25e34-7e4d-43a5-b37e-96f8be1ab1af)

#### About Us

Swagelok is a $2B developer of industrial fluid system products and services. Swagelok Edmonton is an authorized Swagelok Sales and Service Centre serving Canadian companies in clean energy, chemical, oil and gas, and other industries. Proud member of the Canadian Council for Aboriginal Business.

Tel: [780-437-0640](tel:7804370640).

Swagelok Edmonton values your privacy. This website uses cookies to enhance user experience and analyze performance and traffic. Our policies are posted [here](https://edmontonvalve.swagelok.com/policies).

[Login/Register](https://products.swagelok.com/en/register) | [Privacy](https://www.edmonton.swagelok.solutions/policies?hsLang=en) | [Safe Selection](https://www.swagelok.com/en/Safe-Product-Selection) | [Centre Locator](https://www.swagelok.com/en/locate-a-sales-service-center) | [Sitemap](https://edmonton.swagelok.solutions/sitemap.xml) | [Legal](https://www.swagelok.com/en/Legal-notice)<https://www.edmonton.swagelok.solutions/policies?hsLang=en>

© 2012-2024 Edmonton Valve & Fitting Inc.