Share this
Steam Separation Increases Quality for Your Fluid System
by Taryn Hardes on Wed, Nov 13, 2013 @ 15:11 PM
Three different designs remove water from vapour for better performance
![]() |
| The Baffle-Type Separator,Centrifugal Separator, and Mechanical Coalescing Separator. |
The efficiency of any steam system depends largely on the quality of the steam that's delivered to the process equipment. The goal is 100 percent vapour and no liquid, also known as saturated steam. Anything less can cause problems. In a steam turbine, for example, moisture will erode the internal parts. In heat-transfer units, entrained moisture will increase the condensate film on the heat-transfer surface, which can reduce heat-transfer performance efficiency by 14 percent or more.
If a steam system is properly designed, specified, installed, operated, and maintained, it should operate with steam at or close to 100 percent. Proper steam velocities will allow the moisture to drop out of the steam vapour to the bottom of the pipe, where a drip leg steam trap station can remove it. But not every system can always operate under ideal conditions. That's the time to use a steam separator, sometimes called a moisture separator.
A steam separator takes advantage of the inertia difference between condensate (liquid) and steam (vapour). They do that by creating a pressure drop across the device. The design of the separator determines the amount of pressure drop.
Three types
There are three basic types of steam separators: baffle, centrifugal and mechanical coalescence. Often, a combination of two different types of separators is used to achieve higher efficiencies.
The baffle-type separator consists of one or more internal baffles that redirect the steam in one or more different directions. This allows the heavier condensate droplets to be removed by a control valve or steam trap station. This is the simplest separator to design and manufacture, but it also is the least efficient.
A centrifugal separator, as the name implies, uses centrifugal force to separate the condensate from the vapour. The steam is directed into a steam-flow pattern resembling a spinning cyclone. The heavier condensate is expelled to the wall of the separator then drained by gravity to the condensate collection point. The steam pressure drop across this type of separator tends to be larger than in the other types because the velocity required for operation is larger. Less centrifugal action will decrease its performance. It's especially important, therefore, to determine the effect a pressure drop might have on the rest of the system.
The mechanical coalescing steam separator uses a two-stage process. In the first stage, the steam is introduced to a stainless steel mesh that makes the steam flow change directions. Fine water particles combine (increasing their size and mass), fall by gravity to the bottom of the separator, and are removed through a drain device. Any droplets that are not removed are directed to a second, centrifugal stage. In the second stage, deflector blades separate all the condensate droplets from the steam flow and on to a drain. The mechanical coalescing separator is usually the preferred design because it is not flow dependent and has a high efficiency factor. Also, it has a relatively low pressure drop compared to the other two designs.
You can read more detailed information about steam separators online, courtesy of Swagelok Energy Advisors. Then give Edmonton Valve and Fitting a call to discuss how we can help you get the setup that's best for your system.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)