Share this
It's That Time Again: Start Winterizing Your Fluid System Now
by Taryn Hardes on Tue, Oct 15, 2013 @ 14:10 PM
To avoid unplanned downtime and labour, get the work done while it's still warm
|
Edmonton Valve's SEA expert Tristian McCallion. |
Did you notice a few cooler days in the Edmonton weather forecasts this month? That's your reminder that winter is not far off. This is the time to get your systems ready for cold weather, and Edmonton Valve and Fitting wants to help.
Last year we presented three winterization webinars that we recorded and put online. Our resident expert on the topic, Tristian McCallion, guided his audience through the best practices of steam tracing, steam trap stations and unit heaters.
Each video is about 45 minutes long and packed with way more information than we can summarize in a blog post, but here are a few highlights:
Steam tracing
The most efficient type of tracing is the gut line, in which the tracer runs inside the pipe. The entire exterior surface of the trace line is exposed to the process fluid, so you get great heat transfer. But it's very difficult to install and maintain, so you don't see gut lines used very often.
Another method is the jacketed design. In this case, the tracer is on the outside, surrounding the pipe. It's not as efficient as a gut system because some heat radiates outward.
The most common design used today is the bare-tube tracer. It's very easy to install, very easy to change, and very reliable. The downside is that it is not nearly as efficient. Having said that, there are ways to improve efficiency. A heat-transfer material can help, such as a heat transfer cement.
Remember, heat rises, so put the tracers on the bottom of the pipe for maximum effect. It's also important to keep tracers in good repair. They may not use much energy individually, but when you add them up the total can be significant.
Steam trap stations
You'll want a steam trap station at the bottom of the supply header to remove any condensate that builds up, and on the return header. Avoid threaded systems if you can. The expansion and contraction inherent in the system is a setup for leaks. It's also important to keep the supply and return headers as close together as possible. If they are close enough, it usually takes only one person to start up the system or take it down.
The steam trap station itself has several components. One important part is a strainer. One of the main reasons that traps fail is because of dirt or corrosion in the system. It's also important to have a blow-down valve on the strainer. One more component is the test valve, or the secondary isolation valve. There are several ways to test steam traps: temperature, ultrasound and visual tests. McCallion recommends using all three. Each is good for indicating certain problems, and each has its negatives.
Unit heaters
Unit heaters are often ignored when it comes to winterization. But if they are installed and maintained correctly, they can be a very efficient way of heating a large industrial space. One of the biggest problems we run into is that the heat is not being distributed correctly. That's usually a matter of properly adjusting louvers. It's also important to make sure areas are not being cut off by other pieces of equipment. A combination of vertical and horizontal heaters usually is best.
"People understand they have to winterize, but most of the time it becomes a reactive procedure rather than proactive," McCallion says. "Really, you should already have the work done by the time you start thinking about bringing your winter jacket out."
About Swagelok Energy Advisors
Swagelok Energy Advisors has a core team of four full-time field engineers in North America. They’re on the road three out of every four weeks. In 2011 they conducted 62 steam system reviews, held 26 training events and worked on two large implementations. When needed, they can call on local specialists like Tristian McCallion, here at Edmonton Valve & Fitting.
Most of these experts are mechanical engineers with 15 to 20 years of working with steam systems in a variety of industries. Not only do they know steam, they know how it is applied in various processes. They understand pulp and paper mill equipment, food processing, refineries and more. So even if it is a new process, they understand what is going on inside the system. Swagelok Energy Advisors won’t just tell you that you need a valve in a particular spot, they’ll explain why.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)