Share this
Bend Swagelok Tubing Using Our Hand Tube Bender
by Taryn Hardes on Tue, Mar 18, 2014 @ 14:03 PM
Using a new tool can be intimidating. Here, we have tips and a video on how to successfully bend tubing using the Swagelok hand tube bender.
![]() |
|
|
A hand tube bender could be the solution for all your tube bending needs. Download the Hand Tube Bender Manual for more details. |
For consistent, high quality bends in tubing made from most materials, all you need is a Swagelok hand tube bender. It bends tubing from 1/8 inch to 1/2 inch in a variety of wall thicknesses. This hand tube bender can be used to form single, offset and other bends in tubing that is fully annealed, high-quality seamless or welded and drawn.
Suppose you want to make a 90-degree bend four inches from the end of the tube, followed by a 180-degree bend, with four inches between bends. Here's all that you need:
* A bender corresponding to the tubing size
* A piece of tubing
* A marker
* A protractor (optional)
Easy steps
1. For the 90-degree bend, first mark the end of the tube from which you are beginning the measurements. Measure four inches from that reference mark, and make a mark to indicate the first bend length.
2. Swing the short handle up so that it is above the bender die.
3. Open the tube latch.
4. Place the tube in the groove of the bender die, with the reference mark to the left of the tube latch.
5. Close the tube latch over the tube. This restricts movement of the tube, but still allows for additional alignment.
6. Carefully lower the short handle until the roll dies rest gently on the tube, while keeping the link straight and parallel to the long handle. If the link is not straight and parallel to the long handle, you may get some premature bending.
7. Align the zero on the roll support with the zero on the name plate, with the reference end of the tube to the left of the latch.
8. Align the bend mark with the mark on the roll support that corresponds to the bend angle. In this example, the L corresponds to 90 degrees.
9. Slowly push the short handle down until the zero on the roll support reaches the 90-degree mark on the name plate. Notice that the tubing will spring back slightly after the bend has been completed. To adjust for spring-back, lift the bender handle and repeat the alignment of the tubing with the roll support, then measure the bend with the bender scale. Bend an extra two or three degrees as needed.
10. After completing the bend, swing the short handle up and away from the tube.
11. Pull the tube latch off the tube.
12. Remove the tube from the bender groove.
13. Measure the bent tube against the protractor or some other object of a known angle to make sure you got it right.
One more time
For the 180-degree bend, you'll follow the same basic procedure, with a couple of extra steps.
Make a mark four inches from the vertex of the 90-degree bend, then draw a line through that mark to indicate the outside or "heel" of the 180-degree bend. This will help you make sure you bend the tube in the direction you want. Follow steps 3 through 8 as listed above. At step 9, after you have reached the 90-degree mark, loosen the short handle from the clevis until the short handle will swing without moving the roll support.
Swing the short handle up until it is slightly above perpendicular to the long handle. Now retighten the short handle. This will provide continuous right-angle leverage for the rest of the bend. Continue the bend until the zero on the roll support reaches the 180-degree mark on the name plate. After completing the bend, swing the short handle away, pausing when the zero on the roll support reaches approximately 90 degrees. Loosen the short handle and move it until it's parallel with the long handle, then retighten the short handle.
Move the short handle up and away from the tube, pull the tube latch off the tube, and remove the tube from the bender groove. You can verify the bend angles using a template or some other object with a known angle.
If that seems like a lot of steps, it may look a bit easier if you watch someone go through them. Take a look at the Swagelok How-To video here.
If you want to immerse yourself in the subject, download Swagelok's Hand Tube Bender Manual. It dives deep into some of the finer points of tube bending, such as "gain" calculations. That's the adjustment you need to make to compensate for the fact that the length of tubing in a radiused bend is always less than if the bend were a sharp 90 degrees. The manual has a full table of fractional adjustments depending on the angle of the bend and the outside diameter of the tube.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)