Share this
Matching Type to Function: A Swagelok Valve Tutorial
by Katie Dennis on Wed, Apr 23, 2014 @ 15:04 PM
We'll walk you through the steps, starting with 'What do I want the valve to do?'
When you need a valve for an instrumentation system, the choices may seem overwhelming: ball valves, check valves, excess flow valves, fine metering valves, multi-port valves, needle valves, relief valves -- the list just keeps going. And each of these valves comes in many sizes, configurations, materials and actuation modes.
There's an article in a recent issue of PROCESSWest magazine that can help you sort through options and make the best choice for your particular needs. Not surprisingly, the author is from Swagelok. Mike Adkins is an industry expert when it comes to valves and regulators.
Adkins says the best place to start is with the most basic question: What do I want the valve to do? Is it simply an on-off function, or do you need to control the flow? Some fine metering valves are not designed to shut off at all. Do you need to control a thick fluid, a thin fluid or a gas? Do you need to make sure the fluid goes in only one direction?
On/off (ex: 60 Series)
![]() |
|
| 60 Series Ball Valve |
On-off control is the most basic valve function. Valves in this category stop and start system fluid flow. Primary on-off valves are ball, gate, diaphragm, and bellows valves. Perhaps the most common of all valve types, ball valves can turn the flow on and off with just a quarter-turn of the handle. The ball has a large hole through its centre. When the hole is lined up with the flow path, it's wide open. Turn it 90 degrees, and the flow is completely stopped. Swagelok's 60 series ball valves are designed for reliability and low maintenance. They feature a unique coned-disc, spring-loaded seat; live-loaded, two-piece chevron stem packing; and three-piece, swing-out design, 3-piece process/instrumentation.
Flow control
(ex: 26 Series)
![]() |
|
| 26 Series Needle Valve |
Sometimes you need the flow to be somewhere between fully on and fully off. For that function, a needle valve is a great option - and we are a needle valve supplier. A needle valve has a long stem with tip in the shape of a thin V, or needle. The fine thread means you can turn the handle to get a precise desired flow, and it will stay there reliably. Swagelok's 26 Series is one of many Swagelok needle valves that can fit the bill.
Directional flow
(ex: CH Series)
![]() |
|
| CH Series Check Valve |
Some applications require a valve that ensures flow in only one direction. Those are called check valves. Did you know Swagelok is a check valve supplier? In most designs, the upstream fluid force cracks open a poppet, allowing flow. When there's an increase in downstream of back-pressure force, the poppet is forced back into its seat, preventing reverse flow. Swagelok's CH Series valves come with a variety of end connections, and with cracking pressures of one-third PSI to 25 PSI. That's 0.03 bar to 1.8 bar.
Overpressure protection
(ex: R Series)
![]() |
|
| R Series Relief Valve |
Too much pressure can damage a fluid system. Overpressure protection valves do exactly what the name says, preventing the build-up of pressure beyond a certain setting. They come in two types, rupture discs and relief valves. Rupture discs are used primarily on sample cylinders. A metal diaphragm ruptures when pressure gets too high, venting to the atmosphere. Obviously, it's good for only one use. A relief valve is more sophisticated, using a spring-loaded poppet for measured release of fluid, and closing back up when pressure falls back below the set level. Swagelok R Series proportional relief valves can be set at pressures from 10 psig (0.68 bar) to 6000 psig (413 bar).
Excess flow
(ex: XS Series)
![]() |
|
| XS Series Excess Flow Valve |
If a downstream line ruptures, the fluid can flow out uncontrolled unless the system includes an excess flow valve. Under normal conditions, a spring in the valve holds a poppet open. When there's excess flow downstream, it trips the poppet into a closed position, stopping almost all the fluid flow. When the system is corrected, the valve returns to its open position. Swagelok's XS Series stainless steel valves have spring loaded actuation, allowing them to work in any orientation. They can handle pressures up to 6000 psig (413 bar) and temperatures up to 204 C degrees.
You can read the Adkins entire tutorial online. Once you have matched the valve type to the function you need, there are still many details to work out. There are installation issues, maintenance schedules, safety code requirements and more. And, of course, you need the valve in the correct size for the pressure, flow rate and temperature of the fluid in your system. To discuss the answers to those questions, call us at 780-437-0640.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)