Share this
How To Optimize Your Fugitive Emissions Plan in Edmonton Refineries
by Tristian McCallion on Wed, Jan 12, 2022 @ 09:01 AM

Fugitive emissions are the bane of any refinery process. Releasing methane contributes to intensifying climate change effects and is twenty to forty times more effective at trapping heat than an equal amount of carbon dioxide over a hundred-year period. While non-toxic, methane in high enough concentrations can cause asphyxiation and becomes flammable in air mixtures beginning at 5.4% volume. Under MERR, an individual or corporation found noncompliant with Directives 017 and 060 is liable for fines up to $50,000 and $500,000, respectively.
The oil and gas industry is responsible for 44% of Canada’s methane emissions, and in Alberta, this value is over 70%. To slash methane emissions 40-45% to 2012 levels per the Pan-Canadian Framework on Clean Growth and Climate Change, every step of the refinery process must be evaluated and updated with state-of-the-art equipment to seal, mitigate, and detect leaks. For any fugitive emission plan, the best tools will be leak detection services, hose evaluations, and emission-reducing components.
New Regulations for an Existing Fugitive Emission Plan
Three regulations to identify, analyze, and resolve fugitive emissions have already gone into effect in 2020: an upper limit on compressor venting, leak inspection, and a ban on venting for completed wells via hydraulic fracture. Two more regulations, venting limits on general facilities and pneumatic devices, are set to go into effect on January 1st, 2023. With slightly over a year to begin complying with stricter standards, here’s a noncomprehensive list of possible fugitive emission sources to consider:
- Venting of casing heads
- Flash emissions from storage tanks
- Well completions, blowdowns, and workovers
- Compressor rod packing
- Venting from reboilers
- Plant leaks
- Pneumatic devices
- Venting of gas for maintenance/repair
- Pipeline leaks
- Seal oil degassing
- Leaks from mains and service lines
- Leaks at metering stations
- Pipeline blowdowns
Valves as a Major Contributor to Fugitive Emissions
Sixty percent of all fugitive emissions can be attributed to valve stem leaks, and reviewing the potential thousands of valves over the refinery process is a daunting task. One important distinction in evaluating valves is their state of actuation: occasional or continuous. Visual inspection for damage to the gland studs or stem can identify valves on the verge of mechanical failure; the failing studs or stem can pierce the packing, causing leakage. Different temperatures, pressures, and media could also be a source of rapid wear; in general, the more often a valve is operated, the faster it is likely to wear. Furthermore, different valves will have different characteristics in valve actuation force, such as axial compression to radial compression ratio, friction, and adjustability. Note that valves with rising stems are likely to leak more frequently than quarter-turn valves.
Valves need not only be mechanically sound but also properly installed to combat fugitive emissions. Correct installations will provide additional compression to the packing, further lowering emissions and lengthening the valve’s service life.
An Overlooked Source for Fugitive Emissions
Hoses and other open-ended lines account for 5-10% of fugitive emissions on the high-end of estimations. This may seem insignificant compared to valves, but it is important to remember that any opportunity to reduce emissions saves money by conserving a valuable fuel source and reducing the buildup of potent greenhouse gas in the atmosphere. Given that leaks from hoses often occur in direct contact with the atmosphere, these fugitive emissions have a chance to resolve into a highly flammable mixture. Properly functioning equipment may undergo leakage when techniques are incorrectly applied to the line, such as a block and bleed procedure.
Maintaining Seal Support Systems to Combat Fugitive Emissions
When considering seal support systems and their possible contribution to fugitive emissions, the separate maintenance requirements of static and mechanical seals will come into play. Static seals involve not only the gasket itself but the joint at which it is affixed. In joint failure, some aspect of the flange-fastener-gasket system fails. Common causes of failure include incorrect tightening or application of fasteners, reuse or incorrect gasket application, and user error in installation. These failure modes will manifest physically as corrosion, stress-cracking corrosion, fatigue, and self-loosening seals.
Mechanical seals evolved as an industry response to greater demands in emission standards. While most low-emission regulations can be covered by mechanical seals, seal-less pump drive options do exist for the most exacting emission conditions at a tradeoff of pump efficiency. Generally, seal-less systems see utilization in a lock-and-key manner: a highly specific application, but the most overall efficient for that particular process.
Reinforce Your Fugitive Emission Plan with Edmonton Valve & Fitting
Edmonton Valve & Fitting offers a plethora of products and services to keep your Edmonton refinery running efficiently while adhering to new and evolving fugitive emission standards. For the needs of today and tomorrow, our Field Advisors can bring your operation’s fugitive emission plan to fruition.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)