Share this
How To Reduce Fugitive Emissions with Valves for Better Compliance in Alberta
by Thomas Webster on Tue, Jan 04, 2022 @ 13:01 PM

Regulatory requirements and increasing focus on environmental, health, and safety concerns have made fugitive emissions reduction one of the hottest topics in Alberta oil and gas operations. Fugitive emissions come from countless sources, but valves are the most common. In a typical industrial facility, approximately 60 percent of fugitive emissions come from valves.
Valves present the greatest point of leakage in any system. Preventing fugitive emissions with low-emission valves is a high priority, and not just because of regulations—emissions hurt profitability by leaking valuable products, not to mention the risks to health and safety. Fortunately, these risks can be mitigated by developing a fugitive emissions management plan that includes high-quality valves designed for low emissions.
Risks of Fugitive Emissions from Valves
Fugitive emissions can have major consequences for the health and safety of the environment, your people, and your business. Some of the risks and effects include:
- Contribution to climate change
- Environmental pollution
- Health problems resulting from long-term exposure to harmful gases
- Fire and explosion hazards
- Market-based incentive under Greenhouse Gas Pollution Pricing Act: facilities that are less efficient have to pay, while those that are more efficient gain credits that can be held or sold
- Repair is not enough: detected potential leak points are subject to fines
- Financial losses resulting from lost product and downtime
The Fire Triangle
The “fire triangle” (pictured right) shows the three elements needed to ignite a fire: oxygen, fuel, and heat. Oil and gas facilities can mitigate the risk of fires by removing or limiting one or more of those elements; for example, by keeping all fuel sources free of oxygen. However, fugitive emissions release flammable gas into the atmosphere, mixing with oxygen and forming two legs of the fire triangle. If concentrations of emitted gases are high enough, a small spark can ignite a fire or cause an explosion.
The Cost of Lost Product
Oil and gas producers in Canada lose over 30 billion cubic feet of methane gas to fugitive sources every year. This means billions of dollars of valuable product is lost forever. In addition, regulatory penalties can make the financial impact even harder if fugitive emissions don’t comply with regulations. End users face increased economic costs in these scenarios—inefficiency that hurts any operation’s bottom line.
Fortunately, there are many cost-effective ways to mitigate fugitive emissions from valves.
Reducing Fugitive Emissions from Valves
Because valves are such a high risk for fugitive emissions, it’s important to use only high-quality valves and prioritize their maintenance and repair. Reliable, low-emission valves can make a huge difference in reducing fugitive emissions across a facility.
Replace Aging Valves
Fugitive emissions often come from older valves that have either worn out, suffered damage, or were designed with older materials or technologies. By thoroughly inspecting and testing valves throughout the facility for leaks, you can identify the main “problem components” and strategically upgrade the ones with the greatest impact.
When upgrading aging valves, make sure to select only the highest quality products, and be sure they are optimized for your specific processes.
Valves from Swagelok to Prevent Fugitive Emissions
Multiple low-emission valves are available depending on your operation’s needs:
- Instrument Ball Valve: For any gauges or instrumentation needs, the 40 Series (including the 40G and 40T/40E lines) are available with API 641 Certification. These valves have been tested to emit below the stringent 100 ppmv standard and are available from 1/16- to 3/4-inch sizing.
- Process Ball Valve: This valve is available for piping systems. The 60 Series also are available with API 641 certification and are available in 1/8 to 2-inch sizing.
- Instrument Needle Valve: A needle valve can be used for flow-metering applications. Several styles are available with API 624 low emission certification.
- Double Block and Bleed Valve: This valve combines block and bleed valves for interface with other components, isolates upstream and downstream flow, and is employed in component maintenance/repair/replacement. Depending on the valve type, API 624 and 641 Certification are available.
- 5-Valve Manifolds: These may be used on differential setups and provide the ability to block, equalize, and vent two process conditions.
With so many factors affecting valve performance, it’s important to consult with a valve expert to help you decide what materials and options your process requires.
Follow a Valve Preventive Maintenance Program
Even new, high-quality valves can leak if they aren’t correctly installed and maintained. A preventive maintenance program is an essential part of any fugitive emissions plan to detect small leaks before they become big ones. A valve and fluid system expert can perform an onsite consultation to identify high-risk components and help set up an effective preventive maintenance program.
Get Expert Help Reducing Fugitive Emissions from Valves
Fugitive emissions from valves pose risks to health, the environment, and your bottom line. Edmonton Valve & Fitting understands the importance of reducing fugitive emissions and is here to help you select valves to make your facility safer and more efficient. To ensure you’re getting the best possible components for your system, one of our Field Advisors can perform an onsite evaluation and provide recommendations for emissions-reducing valves.
Swagelok valves, without design modification or special ordering instructions, passed the API Low-E test for fugitive emissions. By using Swagelok valves, you meet and exceed the strictest standards in the industry and keep your people, equipment, and products safe. Plus, using Swagelok valves means your components are protected by Swagelok’s industry-leading Limited Lifetime Warranty.