Share this
How Do Gas Pressure Regulators Work?
by Thomas Webster on Tue, Feb 01, 2022 @ 09:02 AM

Working with gas pressure regulators can be daunting if you’re new to the field. Regulators handle the important task of keeping a system operating at maximum efficiency while avoiding a dangerous buildup of pressure. Unchecked, this buildup could cause a rupture to equipment, costing downtime and maintenance as well as posing a risk to operators. To answer the question “how do gas pressure regulators work?”, it’s important to understand both the mechanisms and function of the devices, design style, and how to troubleshoot some common issues.
How Do Gas Pressure Regulators Work: The Basics
Pressure regulators operate under the concept of a system in equilibrium. With the exception of instantaneous changes, axially-aligned forces must vectorially sum to zero for the system to dynamically respond and remain balanced. In real-world applications, both the sensitivity and precision of the equipment must be considered to determine how quickly the sensor can restore itself to mechanical equilibrium. To answer the question “how do gas pressure regulators work?'', it is best to start by describing what comprises a gas pressure regulator. Regardless of style, regulators consist of three distinct components:
- Loading mechanism: Responsible for a force antiparallel to the inlet/outlet pressures. A screw-adjustable spring or gas-fed dome provides the force; in some designs, a combination spring and dome load are utilized.
- Sensing mechanism: The barrier between the load force and inlet/outlet pressures. This mechanism is able to sense changes in pressure and act to restore the displacement from equilibrium. Physically, it exists as a diaphragm for low-pressure, spring-loaded regulators and all dome-loaded regulators or a piston for high-pressure, spring-loaded applications.
- Control mechanism: A poppet is used to reduce high inlet pressure to lower outlet pressure. The poppet can either be balanced or unbalanced. The balanced design features an orifice through the poppet which reduces the area on which the inlet pressure can act. A balanced poppet is less susceptible to the effects of dependency, where outlet pressure can change seemingly paradoxically to a change in inlet pressure. Meanwhile, unbalanced poppets see usage in smaller regulators and low-pressure environments.
The operation of the gas pressure regulator follows the flow of the inlet and outlet pressure. This is sampled continuously by the sensing mechanism and balanced against the loading mechanism. Depending on the type of gas pressure regulator, the poppet will either open or close to regulate inlet or outlet pressure. The damping level of the regulator also plays an important role in selection. An underdamped regulator may be susceptible to ringing due to a rapid, sudden change in inlet pressure, while an overdamped regulator could exhibit hysteresis (a dependency on prior system states).
Pressure-Reducing or Back-Pressure Regulator?
As important as the construction and mechanics of a gas pressure regulator is its type: pressure-reducing or back-pressure. Pressure-reducing, as one may deduce, reduces an inlet pressure to a fixed preset outlet pressure. The poppet defaults to an open position to allow pressure to flow from inlet to outlet but closes to reduce outlet pressure when inlet pressure increases beyond the fixed outlet pressure value. The pressure-reducing regulator is installed upstream of sensitive equipment as a means of protection.
In contrast, the back-pressure regulator’s role is to maintain the inlet pressure below a preset value. The poppet’s position is normally closed, but the poppet can toggle between an open or closed position to release or build pressure, respectively. As its role is to maintain inlet pressure, the back-pressure regulator is installed downstream from the components it protects.
Due to their alternate placement in systems around sensitive equipment, pressure-reducing and back-pressure regulators may face unique difficulties during use. While the following list is not inclusive of every challenge an operator could encounter, being able to correctly diagnose these issues will help reduce maintenance downtime.
- Accumulation: A condition of back-pressure regulators whereby inlet flow causes an increase in inlet pressure
- Creep: An increase in outlet pressure, genuinely due to leakage of the regulator seat
- Droop: When outlet pressure decreases in a pressure-reducing regulator following an increase in flow rate
- Lockup: When Outlet pressure increases as flow rate decreases to zero
- Supply pressure effect: A change in the outlet pressure opposite the direction of a change of inlet pressure in pressure-reducing regulators; also known as dependency
Have an Expert Vendor Answer Your Pressure Regulator Questions
Gas pressure regulators play a key role in protecting your equipment and workers. For questions beyond the introductory “how do gas pressure regulators work?”, you can contact one of our Field Advisors for an in-depth consultation of your specific system and pressure regulators that will keep your operation running smoothly.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (28)
- Downloads (25)
- Resources (25)
- Tubing (25)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- September 2026 (1)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)