Share this
How Gas Distribution System Design and Fabrication Can Improve Plant Efficiency
by Thomas Webster on Mon, Jul 11, 2022 @ 09:07 AM
.jpg)
In a gas processing plant, efficiency is everything. When something goes wrong with a gas distribution system, it has to be fixed as quickly as possible—which unfortunately often means cobbling together a fix or replacement from whatever is available.
The problem is that by using disparate parts from multiple suppliers within a system, it tends to lose efficiency and become more complex than necessary. A more effective solution is a complete system engineered for the specific application from a local vendor specializing in gas distribution system design and fabrication.
Key Aspects of Gas Distribution System Design and Fabrication
In most plants, gas distribution system design and fabrication can be divided into four main subsystems: the source inlet, gas panel, changeover, and point-of-use. It is important that every part of the system operates reliably and efficiently, as a failure at any point has the potential to cause problems downstream.
Swagelok Source Inlet (SSI)
The first stage of the gas distribution system design is the source inlet. The source inlet connects a pressurized gas source to the rest of the system. It can be as simple as a single hose connected to a cylinder or a complex manifold or system of hoses and valves.
The source inlet may seem like a simple set of components, but it’s one of the most critical points in the system. As the most upstream point in the process, any leakage, and pressure loss at the source inlet trickles down to the entire system—so a reliable, engineered solution is essential. A gas distribution system design and fabrication expert can evaluate your process and determine the exact types of components that will ensure reliability and efficiency. These might include isolation valves, individual vent or purge lines, or other options.
Swagelok Gas Panel (SGP)
After the source inlet, gas flows to the gas panel, where the system pressure and flow rate are controlled. The gas panel uses either a single- or double-stage regulator arrangement to control pressure, depending on the application details.
Designing the gas panel—especially the pressure regulator selection—is another critical part of gas distribution system design and fabrication. Because the pressure regulator is the heart of the whole system, it’s very important that it is optimized for the application pressure, fluid properties, and the rest of the system components. Selecting a pressure regulator for a gas distribution system is a sophisticated task that is usually best left to an expert.
Swagelok Changeover (SCO)
The changeover system switches from one gas source to another when it runs out (or reaches a set changeover pressure). Changeovers can be partially or fully automated. The safest, most efficient option is an automatic changeover that keeps the gas flowing at constant pressure as it switches sources, allowing the system to operate continuously.
Of course, the more automated the changeover is, the more critical the engineering details become. This is another point where it’s unwise to cobble together a fix from disparate parts. A gas distribution system design and fabrication vendor will be able to determine the most efficient way to implement a changeover in your system, depending on the source type and process conditions.
Swagelok Point-of-Use (SPU)
The final downstream point of the gas distribution system is at the point-of-use where gas is dispensed. There are usually many point-of-use stations in a plant, and they may have different design and operation requirements. That being said, they are typically the least complex part of gas distribution system design and fabrication.
The point-of-use station is the last point where gas pressure is controlled before it is dispensed. A point-of-use station typically includes a pressure regulator, pressure gauge, and isolation valve to allow precise gas pressure adjustment.
Even though point-of-use systems are relatively simple, they must still provide reliable, consistent, and safe operation. Engineering a station with a compact design and custom mounting options can maximize space while making the station as easy and safe to use as possible.
Gas Distribution System Design and Fabrication Solutions for Northern Alberta
In Northern Alberta gas processing plants, efficiency is critical—and a “Frankenstein” system consisting of disparate parts just doesn’t cut it. Luckily, Edmonton Valve & Fitting has decades of experience in efficient gas distribution system design and fabrication, so custom-engineered solutions are available.
Our Field Advisors can evaluate and optimize your existing gas distribution system and recommend quality Swagelok components that can improve safety and efficiency. Or, we can provide design support for a custom gas distribution system from the ground up to optimize your gas handling applications. Our gas distribution system design and fabrication services include standardized, modular systems and industry-leading Swagelok components customized to your application.
To find out more about Edmonton Valve & Fitting’s gas distribution system design and fabrication solutions, contact us through our website or by calling 780-437-0640.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)