Share this
Considerations for a Hydrogen Plant in Canada: Design Factors That Cannot Be Overlooked
by Thomas Webster on Tue, Nov 09, 2021 @ 15:11 PM
.jpg)
Alberta, Canada is on its way to becoming a significant hydrogen hub. As more hydrogen plants and pipelines are built in Canada, design considerations specific to hydrogen service will become increasingly important.
Good hydrogen plant design is necessary to ensure worker safety and equipment reliability. Here, we’ll look at some often overlooked hydrogen plant design considerations, like component and material selection, and why they are critical for any hydrogen plant design in Canada.
Properties of Hydrogen
Proper hydrogen plant design requires an understanding of hydrogen’s properties. By taking advantage of these properties, a facility can be designed to minimize hazards.
Hydrogen gas is non-toxic, non-poisonous, colorless, odorless, tasteless, and generally undetectable by human senses. While these properties mean it is usually not a safety concern, it makes leaks challenging to detect. Hydrogen is not harmful to humans directly, but it can create significant hazards under certain conditions.
Flammability
Hydrogen’s flammability range is vast compared to other gases, and the energy required for combustion is much lower. In other words, it only takes a tiny spark to ignite a hydrogen fire.
When it ignites, hydrogen burns with a nearly invisible pale blue flame that produces no smoke. In addition, hydrogen flames have low radiant heat, so you may not feel any heat unless you are very close to the flame. These characteristics can make it easy for hydrogen fires to go unnoticed without the aid of sensors such as thermal imaging cameras.
Buoyancy
Hydrogen is the lightest molecule in the universe, so it rises quickly when it leaks into the air. This can help mitigate the dangers of hydrogen leaks as the leaking hydrogen will not accumulate at the ground level where workers are. However, in enclosed spaces, it accumulates in-ceiling pockets, mixing with air and potentially creating an explosive mixture. Proper ventilation is essential to prevent this hazard.
Embrittlement
Hydrogen is a tiny molecule that readily diffuses into many materials, especially under pressure. This can lead to reduced tensile strength, ductility, and increased fatigue crack propagation rate. This phenomenon is known as hydrogen embrittlement, and avoiding it requires careful selection of hydrogen-compatible materials for every component.
Hydrogen Plant Design Considerations
Hydrogen’s unique properties require unique design considerations. To reduce the risk of the hazards described above, follow these best practices:
Use Only Hydrogen-Compatible Materials
ASME B31.12 Standard on Hydrogen Piping and Pipelines provides material selection requirements and recommendations for hydrogen service. Austenitic stainless steels like 304 and 316 are recommended for all components in hydrogen service, and they should be used in the annealed condition if possible.
Some carbon steels can be used for gaseous hydrogen service if operating temperatures are at least -29°C. Still, they are not recommended for high-pressure applications, as they are more susceptible to embrittlement than stainless steel.
Aluminum alloys, copper, and copper alloys are also generally suitable for hydrogen service. However, nickel and nickel alloys are susceptible to severe hydrogen embrittlement and should never be used with hydrogen.
Prevent Leaks by Minimizing Joints
Because of its small molecular size, hydrogen leaks extremely easily. To limit potential leak points, piping and tubing should have the minimum number of joints possible. Where fittings are used, they must be suitable for hydrogen service and specific operating conditions. Welded fittings are preferred for piping systems as they have a lower potential for leaks than mechanical fittings.
Swagelok FK-series fittings are some of the only tube fittings engineered for the unique demands of hydrogen applications, with 316 stainless steel fabrication and pressure ratings up to 22,500 psi. In addition, SWS weld system are another valuable tool for hydrogen gas service in Alberta. These fixtures allow the welding of a gas-sealing connection that is an effective solution for hydrogen sealing.
Eliminate or Minimize Fire Hazards
To minimize the risk of a significant hydrogen gas release inside the plant, hydrogen gas should be supplied from an outdoor area at a safe distance from structures, ventilation intakes, and vehicle routes. When hydrogen is used indoors, it should be stored outdoors if possible and supplied to the indoor area using welded piping.
If hydrogen cylinders must be placed indoors, take the following precautions to prevent hazards:
- Limit the total hydrogen volume based on workspace size.
- Store hydrogen cylinders away from cylinders containing oxidants.
- Keep cylinders secured.
- Use only non-combustible materials for plant infrastructure.
- Set up ventilation systems to introduce air low to the floor and exhaust at the room’s highest point.
- Install hydrogen sensors throughout the plant.
- Install dispensers in unconfined areas with ceiling heights of at least 7.5 meters.
For High-Quality, Hydrogen-Compatible Components and Systems, Look to an Experienced Vendor
Edmonton Valve & Fitting offers a wide range of hydrogen-compatible Swagelok components with top-quality metallurgy, leak-tight designs, and high-pressure resistance. We also offer EC-79-certified components suitable for on-vehicle applications, heavy-duty, rail, ship, and aerospace.
Our Field Advisors can also perform an onsite consultation to assess your hydrogen plant’s needs and recommend the best systems and components to ensure safe, reliable operations. Field Advisory Services include, but are not limited to:
- Virtual onsite evaluations
- Design advice
- Leak detection and repair
- Product-specific training
- Component and instrumentation advice
- Regulator sizing guidance
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)