Share this
Hydrogen Plant Fire Protection & Safety Starts with Leak Mitigation: Top Solutions for Alberta-based Operations
by Thomas Webster on Tue, Dec 21, 2021 @ 09:12 AM

In general, fires are incredibly easy to recognize: the bright color, the billowing smoke, and the intense heat. An odourless, smokeless, and colourless flame in broad daylight with low emissivity—these are challenges faced in detecting a hydrogen fire. Additionally, as the smallest of all diatomic molecules, H2 requires special materials to avoid embrittlement and leakage during storage or transportation. A further complication is hydrogen’s buoyancy, which allows it to accumulate undetected in the ceilings of closed facilities, potentially leading to catastrophic results.
Hydrogen mixes readily with air and produces a flammable mixture in volumetric ratios as little as 4%, and mixtures can be ignited with less than a tenth of a millijoule of energy. Owing to its low molecular weight and high diffusivity, hydrogen-oxygen has a greater burn velocity than similar hydrocarbon mixtures, which increases the risk of a burning fuel transforming into an explosion.
The economic loss cannot be understated: system leaks could lead to a hazardous environment for workers and equipment, and an overall reduction in efficiency. While detection systems and sensors form an important bulwark of hydrogen plant fire protection, the best defense is ensuring your system has the correct components necessary for the complex demands of hydrogen fuel. Solutions for H2 storage and transportation—including low leak valves and seal flush systems—are discussed below.
Certified Components for Hydrogen Plant Fire Protection
While hydrogen leaks will generally occur at any seals or fittings, valves are not exempt. Regulation EC-79 has outlined necessary considerations and requirements for components used in hydrogen-powered vehicles, but can be extended to the greater infrastructure of hydrogen production, transportation, and storage. All EC-79 certified valves must be subjected to the following tests as laid out by Annex III (liquid hydrogen) or Annex V (hydrogen gas):
- Pressure test - valves must withstand a pressure higher than the expected working pressure without experiencing material fatigue or failure
- External leakage test - valves must not show evidence of porosity
- Endurance test - valves must exhibit continued operation for a specified number of test cycles
- Corrosion resistance test - valves must resist specified corrosive agents
- Resistance to dry-heat test - valves are exposed to air at maximum operating temperatures
- Ozone ageing test - valves are exposed to air with high ozone concentration
- Temperature cycle test - valves experience a temperature cycle of a specified duration from the minimum operating temperature to the maximum operating temperature
- Hydrogen compatibility test - valves must show no signs of hydrogen embrittlement, including susceptibility to material fatigue and cracking under frequent load cycles
- Seal leakage test - valves must be free from leakage while installed
EC-79 certified valves set a minimum industry standard for safety and reliability. Products carrying this certification have undergone rigorous testing born of the unique concerns of containing and facilitating industrial hydrogen applications.
Controlling Contamination and Lengthening Seal Life
Simply having the right components is only half the battle when it comes to industrial hydrogen applications. With only a small ratio of air necessary to create a highly-flammable mixture, the dangers of contamination are far greater than mere loss of product. High-pressure ratings (from 450 to 5000 or more PSIG) further promote diffusivity and particle interactions, which in a tightly constrained environment could increase the potential for fire or detonation. System servicing becomes a necessity to mitigate and prevent contamination while also lengthening the service life of seals in flush systems.
Beyond extending seal life, seal flush systems help ensure the continued operation of hydrogen systems by reducing downtime for repairs/replacements of critical operating components. Though hydrogen fire plant protection is the primary motivator in safety features such as these, there is real economic value in keeping H2-related industries running with minimal interruptions.
Hydrogen Plant Fire Protection & Safety Options for Alberta Operators
Whether it’s the replacement of old components, an entirely new system, or support for seal flush systems to keep a system running smoothly for as long as possible, Edmonton Valve & Fitting has a multitude of products and services designed for hydrogen plant fire protection and prevention. The safety of your employees and equipment is paramount to the successful operation of any business, and our Field Advisors will keep your H2 systems operating at a high level of safety and efficiency.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)