Share this
Solving Seal Flush Plan 11 Challenges More Easily for SAGD Operations
by Thomas Webster on Wed, Jul 07, 2021 @ 08:07 AM

Seal flush Plan 11 is the most common piping plan used for single mechanical seals in steam-assisted gravity drainage (SAGD) operations. It is simple, inexpensive, and recirculates process fluid from the pump discharge to the seal. In SAGD applications, seal flush Plan 11 may be used for single mechanical seals on pumps ranging from emulsion well pad pumps to export and sales pumps.
Due to the high viscosity of the process fluid (crude oil)—and the use of process fluid to flush the process side of single mechanical seals—challenges with circulation and flow are common in SAGD. Crude oil is highly viscous and is more likely to contain particulates that may clog the seal itself or the flow control orifice, resulting in insufficient flow to the seal chamber. Leakage in seal flush Plan 11 piping can also cause pumping inefficiencies and is typically the result of too many leak points in the design.
Let’s take a deeper look into:
- How seal flush Plan 11 works
- Common challenges associated with SAGD operations
- Potential solutions
Seal Flush Plan 11: An Overview
API Plan 11 is the default flush plan for single mechanical seals and is categorized as a process side plan. This plan utilizes process fluid, recirculating flow from the discharge piping (or another high-pressure section) of the pump through a flow control orifice and to the seal. Seal flush Plan 11 features include:
- Heat removal from the seal chamber
- Prevention of process fluid vapourization
- Self-venting seal chamber (on horizontal pumps)
Considerations for API Plan 11:
- Careful calculation is required to determine orifice size.
- Process fluid containing abrasive solids or polymerizing process fluid should be avoided.
- Proper orifice sizing and throat bushing clearance are required for appropriate flow to the seal.
Seal Flush Plan 11: Common Challenges in SAGD Operations
Two of the most common challenges with seal flush Plan 11 are:
- Plugged seal or orifice
- Leakage in piping connections
Plugged Seal or Orifice
Due to the high viscosity of crude oil involved in SAGD pumping applications, one of the most common issues associated with Plan 11 is plugged seals or orifices. This often results in insufficient flushing and cooling of the seal and can ultimately cause downtime due to mechanical seal damage or failure. Orifice clogging can be confirmed by checking pipe or tube surface temperatures upstream and downstream of the orifice.
Leakage in Piping Connections
When excessive amounts of piping connections are used to route flow from the pump discharge piping to the control orifice and to the seal, leakage is very common. This can result in compromised piping integrity and/or inefficient flow to the seal.
Potential Solutions to Common Challenges
There are a few methods to address issues relating to plugged seals or flow control orifices and leakage. Below, we have detailed potential solutions for each problem.
Addressing Plugged Seals or Orifices
When seals and orifices plug, they can typically be cleaned out. However, when plugged seals or orifices are an ongoing problem, it might be time to reassess process conditions. As the composition of process fluid and water content changes over time, the ability of the fluid to flush and cool the seal can weaken. Recalculating the circulation flow rate, heat removal, and orifice size may show that a different orifice size may be required.
If process conditions do not require a change in orifice size and the seal or orifice continues to clog, it might be necessary to upgrade the seal flush plan. If the cause of clogging is due to solids and particulate matter in the process fluid, a simple upgrade to API Plan 12 is a potential solution. This plan is similar to Plan 11 but utilizes a strainer that is placed prior to the flow control orifice to remove such particulates. This plan also includes pressure gauges on either side of the strainer to monitor for servicing.
If Plan 12 is still insufficient in solving plugging-related issues, a more robust plan that utilizes either a buffer or barrier fluid (as opposed to the process fluid itself) can greatly reduce clogging issues. API Plan 52 is a great starting point when looking to upgrade.
Addressing Leakage in Piping Connections
A simple solution to leakage in piping connections is to make use of fitting kits and specialty fittings that aim to reduce leak points. Every connection should be viewed as a possible leak point. Specialty connectors, such as the extended male connector shown below, can replace threaded pipe connectors, eliminating the leak point altogether.

The Best Solution to Seal Flush Plan 11 Challenges
Edmonton Valve & Fitting has ample experience with seal flush systems for SAGD applications in Alberta and understands the local challenges associated with heavy crude oil. Whether you need help addressing seal flush Plan 11 challenges—or you are looking to upgrade to a more robust solution—our Field Advisors can perform a fluid systems evaluation to determine the best solution to improve seal flush performance and reliability for your SAGD operations. We also offer fitting kits and specialty fittings and connections to reduce leak points and minimize rotating equipment downtime.