Share this
Small Bore Tubing: Streamline Power Plant Maintenance & Enhance Performance
by Katie Reid on Thu, Jan 31, 2019 @ 14:01 PM
Your own technicians can be trained to manage the tube bending and assembly.
Switching to tubing can greatly simplify installation and plant maintenance with any system that delivers steam, condensate, hydraulic fluid, chemicals, pressurized air or other fluids through pipes. For example, rather than 90-degree elbows, you can create gradual sweeps, which minimize pressure drop. To learn more about small bore tubing (up to 2 inches OD) and how it can help with your power plant efficiency, download this free Swagelok PDF:
Suppose you need to service your steam turbine throttling valves, or change out pilot solenoid valves in your electrohydraulic controls. You want to get in and out of the system quickly. Downtime is lost revenue.
But if the systems are hard piped, you are out of luck. Cutting, welding, and threading hard pipe is slow and labor intensive. A better alternative may be stainless steel tubing.
Switching to tubing can greatly simplify installation and plant maintenance with any system that delivers steam, condensate, hydraulic fluid, chemicals, pressurized air or other fluids through pipes, many of which are 2 inches in diameter or less.
You'll save many minutes, even hours, building any typical configuration involving 90-degree turns and other complexities. And with stainless steel tubing, no special contractors or welding teams are required on the plant floor. Your own technicians can be trained to manage the bending and assembly.
Fluid power efficiency
Hard piping systems are inefficient by their very nature. Hard 90-degree turns (elbows) create pressure drop. Threaded pipe fittings are likely to leak, especially if your system generates vibration or thermal expansion and contraction. These leaks can starve your system of pressure.
By contrast, stainless steel tubing is bendable to precise radiuses. You can create gradual sweeps, which minimize pressure drop. And with automated orbital welding, you can greatly reduce the number of potential leak points or mechanical connections. Where mechanical connections are necessary, Swagelok tube fittings will not back off with thermal cycling or high vibration.
Fast assembly
If you have ever worked with stainless steel tubing in diameters of a ½ inch or less, you will find that the larger sizes are no different. Tube cutting, preparation and bending are the same. Tube fittings up to 2 inches fully tighten and seal with one-and-a-quarter turns, just like the smaller fittings.
For permanent connections, the Swagelok orbital welding system will produce precise, repeatable welds and full documentation of the weld quality. The Swagelok orbital welding system, tube benders and swaging units are all available for sale or rental from Edmonton Valve & Fitting.
With stainless steel tubing systems, a best practice is to assemble permanent, welded connections in the instrument and control shop. Then, move the assembly to the plant floor and connect it with tube fittings. If the tube fitting connections are strategically located, then the system becomes modular. When a particular valve or panel needs to be serviced, the tubing assembly is simply detached at the tube fittings and set aside. Then, when service is complete, the assembly is reattached with one-and-a-quarter turns of the tube fitting nuts.
Almost as soon as the last tube fitting is assembled, a tubing system is ready for service. There is no need to flush the system because assembly does not produce filings and chips like a hard pipe system does.
Stands up to stress
Unlike threaded connections, Swagelok tube fittings are highly reliable under a range of conditions, including high vibration and changes in temperature.
A Swagelok tube fitting resists vibration because it is anchored to the stainless steel tubing with two ferrules, which are permanently affixed to the tubing during makeup. The front ferrule performs the sealing function, while the back ferrule grips or holds the tube over a wide area, enabling the tube fitting to resist vibration.
Multiple applications
Many systems in a power plant can become more efficient by switching from pipe to stainless steel tubing, including the chemical feed system, water sampling system, duel fuel systems, generator and lube oil systems, and hydrogen cooling for the generator.
Ready to discuss how small bore tubing can enhance your performance and reduce maintenance? Please get in touch:
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)