Share this
Why Flow Assurance Fluid Characterization Matters for Aging SAGD Wells
by Thomas Webster on Tue, Jun 22, 2021 @ 13:06 PM
Flow assurance fluid characterization is the concept of ensuring fluid flows effectively and efficiently from point A to point B. Originally, flow assurance was a term used to describe the analysis and evaluation of problems resulting from solids forming in pipelines for offshore oil and gas operations. However, flow assurance can pertain to all associated risks with maintaining flow from one point to another for any oil and gas operation.
Steam-assisted gravity drainage (SAGD) utilizes flow assurance analyses during initial drilling of horizontal wells to gain an understanding of what the production well is producing and how the produced fluid (bitumen and water) is flowing from production well to the surface and finally to a processing plant where the bitumen and water are separated. However, like any other oil field, produced fluids from SAGD wells change as the wells age. Flow assurance fluid characterization can help SAGD operators understand the impact of aging wells on the produced fluid, as this affects flow to processing plants as well as the water and bitumen separation process. Below, we will discuss the impact of aging SAGD wells, the importance of flow assurance analyses, and how grab sampling can aid in such analyses.
Flow Assurance Fluid Characterization in SAGD
As SAGD wells age, there are bound to be changes in the produced fluid. It is important to characterize these changes to understand how processes need to adjust over the lifetime of the wells to accommodate. Let’s take a look into aging well characteristics, the importance of flow assurance evaluation for aging SAGD wells, and some methods for maintaining efficient flow and SAGD operations to minimize downtime.
How SAGD Wells Age
After years of bitumen production at SAGD wells, the produced fluid will likely experience a change in the water-to-oil ratio. As the bitumen resource is non-renewable, over years of extraction, the bitumen under the earth’s surface begins to deplete, increasing the size of the cavity. As bitumen depletes and cavity size increases, more steam and heat are required to reduce the viscosity of the bitumen to be able to pump it to the surface. Thus, over time, SAGD wells are likely to produce larger amounts of water and less oil, changing the flow characteristics of the system.
Importance of Flow Assurance for Aging SAGD Wells
As the produced fluid’s water-to-oil ratio changes over time, it is important to quantify such changes, as they are likely to impact the flow properties of the system that may require adjustments to line sizes or pumping requirements. Changes in water-to-oil ratio may require updates to current processes occurring in SAGD operations. After the bitumen and water mixture leaves the production well, it is pumped to the surface to be routed to a processing plant. In the processing plant, this mixture is sent to a settling tank to separate the water from the bitumen. The time required to settle water to the bottom of a settling tank is likely to increase with higher water-to-oil ratios.
If oil is not properly dewatered, this can result in water being passed into the oil lines or pipeline. If temperatures in these pipes are high, water can boil in the pipe, causing increased pressure and thus creating instantaneous backpressure. As the water expands, the flow of oil stops, increasing the oil pressure and forming a slug. As this slug moves through the system, the large mass and high velocity result in a large momentum which may cause damage to supports if the slug collides with an elbow in the piping.
Grab Sampling for Flow Assurance Fluid Characterization
Water-to-oil ratios will inevitably increase as SAGD wells age. It is important to fully understand flow properties and characteristics to make changes to SAGD processes accordingly and prevent unnecessary downtime. A simple and effective method for flow assurance fluid characterization is periodic grab sampling of produced fluid. Grab samples, along with proper instrumentation, provide insight into produced fluid properties, such as viscosity, temperature, pressure, and water-to-oil ratio. Taking regular samples of produced fluid from SAGD wells provides a deeper understanding of how the wells are aging and how the flow through the system is changing. This allows for operators to be proactive regarding necessary changes to SAGD processes that may be required as the properties of the produced fluid change.
Seek Local Fluid Systems Experts
Characterization of produced fluids from aging SAGD wells can provide insight into how the wells are changing over time and how to accommodate such changes. If you are looking to improve SAGD reliability through increased flow assurance fluid characterization, Field Advisors at Edmonton Valve & Fitting can provide an onsite evaluation of your process to determine the best grab sampling solution. Our Field Advisors have ample experience with sampling systems for a wide range SAGD applications and can make suggestions for improving SAGD efficiency.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)



.jpg)