Share this
High Temperature Hydrogen Production: Selecting the Right Components
by Thomas Webster on Thu, Jul 21, 2022 @ 08:07 AM

Hydrogen production doesn’t usually involve the high temperatures and corrosive fluids that can threaten the reliability of equipment in oil and gas refineries. However, high-temperature hydrogen attack, stress corrosion cracking, and hydrogen embrittlement are still concerns, and material selection is critically important. Materials that may be adequate for other operations may be unsuitable for hydrogen operations.
The quality of your components can be the difference that keeps your hydrogen production equipment running safely. In this post, we’ll go over some of the material concerns in hydrogen production, high-temperature hydrogen processes and the challenges they create, and how to choose the right materials and components to keep your hydrogen plant up and running.
Challenges of Hydrogen Production: High-Temperature Hydrogen Attack
While corrosive media and high-temperature processes are normally associated with refineries, not hydrogen plants, there are still potential hazards to watch out for in hydrogen production. High-temperature hydrogen attack (HTHA) and stress corrosion cracking (SCC) are two potential hazards that are especially dangerous because of how difficult they can be to detect.
HTHA occurs in steel exposed to hydrogen under high pressure and temperatures (above 200°C)—like those found within steam-methane reformers. At this temperature, hydrogen dissolves into the steel, where it reacts with the carbon in the alloy. This results in either surface decarburisation, where the reaction draws carbon to the surface of the material, or internal decarburisation, where hydrogen penetrates the steel and reacts with carbon to form methane. The methane cannot diffuse out of the steel, so it accumulates and creates voids in the material, eventually causing cracking.
Surface decarburisation decreases the hardness of the steel near the surface, which is usually not a major concern. However, internal decarburisation can cause serious deterioration of mechanical properties and even catastrophic failure if not mitigated quickly.
Because HTHA is caused by the reaction of hydrogen with carbon, a steel’s susceptibility to HTHA is heavily influenced by its composition. In particular, elements like chromium (Cr), molybdenum (Mo), and vanadium (V) that tie up carbon in stable precipitates help avoid HTHA. Increasing the content of these elements increases the steel’s resistance to HTHA. Likewise, the crystalline structure of austenitic stainless steels makes them resistant to HTHA.
Challenges of Hydrogen Production: Stress Corrosion Cracking
While HTHA is a danger in any high-temperature hydrogen process, stress corrosion cracking (SCC) is not normally considered a major issue in hydrogen production plants. The hydrogen in these processes is much cleaner than that used in refinery processes, but SCC is still possible.
While there may not be large amounts of caustics in the hydrogen production process, even tiny amounts can lead to SCC. Steel piping used in high-temperature steam methane reformers can be susceptible to SCC if there is any place for material to accumulate in the piping system. This is why it’s a good idea to have piping and tubing systems evaluated by fluid handling experts who can identify these points and design them out of the system. Like HTHA, SCC can also be prevented by using corrosion-resistant stainless steels high in elements like chromium and molybdenum.
How to Prevent Equipment Failures with High-Quality Materials and Components
For decades, hydrogen producers have used the Nelson curves in API RP 941 to guide the selection of materials resistant to HTHA. However, HTHA is complex, and failures have occasionally occurred even where the API RP 941 curves did not predict them. For example, the latest revision of API RP 941 (2016) reports 13 new failures below the carbon steel Nelson curve.
Current thought in the industry is that because the Nelson curves can be unreliable, the best approach to preventing HTHA is using inherently safer materials. Furthermore, hydrogen plants should not rely on inspections to detect HTHA, as the cracks are initially microscopic and highly localized.
Avoiding HTHA and SCC failures requires a proactive approach. Once cracks begin to occur, it’s probably too late. Prevent HTHA and SCC failures by following these guidelines:
- Identify all carbon steel components in hydrogen service that present potential hazards in the case of a failure.
- Validate the actual operating conditions (hydrogen partial pressure and temperature) for the identified components.
- Replace all carbon steel components that operate above 200°C and greater than 50 psia hydrogen partial pressure.
- Use inherently safer materials, like steels with higher chromium and molybdenum content.
Inherently Safer Materials for High-Temperature Hydrogen Production
Stainless steel is an alloy of iron, chromium, and other elements. When chromium is added to steel, it forms a surface passivation layer that protects the steel from corrosion. Stainless steel contains between 10.5% and 30% chromium, depending on the type. In general, the more chromium, the better the resistance to HTHA and SCC.
Even within a specific grade of stainless steel, though, there can be considerable differences in properties from one product to another. Most stainless steel is made with the lowest allowed percentages of expensive elements like chromium and molybdenum. Swagelok's stainless steel specifications, however, are at the high ends of the ranges specified by ASTM standards. This means Swagelok components provide better resistance to HTHA and SCC compared to products from other sources—even when they specify the same grade of steel.
Unlike most 304 and 316 stainless steels, Swagelok 304 and 316 are not cross-listable. Many manufacturers sell a stainless steel composition that meets specifications for both 304 and 316. However, because Swagelok’s stainless steels are made to tighter specifications, Swagelok 316 tubing and other components are superior to typical cross-listed 304/316.
Look to Local Experts for the Best Metallurgy for Oil and Gas Corrosion Prevention
If you have questions about which components and materials are best for your hydrogen operations, Edmonton Valve & Fitting can help. Our expert Field Advisors can perform an onsite assessment to understand your process and make sure you get the right components for your process. We can also make specific recommendations regarding piping and tubing system design, instrumentation, and custom components to improve reliability and protect against HTHA and SCC.
In hydrogen production, high-temperature component quality is key to safety and reliability. Our goal is to ensure you have the best available systems and components so you don’t have to worry about the challenges of high-temperature hydrogen production. All our products are backed by Swagelok’s industry-leading Limited Lifetime Warranty, so you can rest assured that you’re covered if anything does go wrong.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (28)
- Downloads (25)
- Resources (25)
- Tubing (25)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- September 2026 (1)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)