Share this
Why an Industrial Fluid System’s Routing Matters More in Alberta, Canada
by Thomas Webster on Thu, Jun 03, 2021 @ 08:06 AM
%20(1).jpg)
When designing facility layouts for oil and gas operations and petrochemical refineries, it is critical to consider industrial fluid systems’ routing, especially in locations like Alberta, Canada. With careful planning and use of prefabricated panels and assemblies, there can be many short-term and long-term benefits.
In the short term, making use of as many prefabricated panels as possible allows ease of implementation during the construction phase or prior to a planned shutdown while cutting down on field labour and saving time in a project’s schedule. In the long term, a well-designed facility with standardization across fluid systems associated with rotating equipment, gas distribution systems, and sampling systems can provide superior consistency and maintainability.
Benefits of Prefabricated Panels and Assemblies for Industrial Fluid Systems’ Routing
Rotating equipment, gas distribution systems, and sampling stations are some of the most important equipment for operations in any industrial facility.
Rotating equipment relies on seal flush systems to protect mechanical seals from damage and prevent seal failure which could result in significant downtime. Gas distribution systems depend on gas panels to reduce the pressure from the gas cylinder in order to deliver the gas to the point of use at the correct flow rate and pressure for a specific application. Grab sampling systems and fast-loop sampling systems are required to inform processes within an operation and can be used to provide quality control for process fluids, plant water, gas supplies, and refined products.
Thus, seal flush systems, gas panels, and sampling systems should be considered during key project planning stages to promote well-designed industrial fluid systems’ routing.
Rotating Equipment
Mechanical seals account for nearly 40% of pumping equipment failures. Mechanical seal failure can be the result of inadequate lubrication to seal faces or poorly configured seal flush systems. Considering the importance of reliable pumping equipment in oil and gas facilities and petrochemical refineries, seal flush systems should not be an afterthought. Instead, it should be in the front-end planning and scope development phase of a project.
Industrial fluid systems’ routing is critical when choosing a seal support system and when planning tubing, piping, connections, and instrumentation locations. Selecting an appropriate seal support system is important for all rotating equipment but becomes more pressing when dual mechanical seals are at play. Selecting the right buffer/barrier fluids for dual mechanical seals is vital in cold weather applications to ensure proper flow rates and pressures even when the fluid is operating at lower temperatures.
Within any seal flush system design, measures should be taken to optimize flow and reduce the likelihood of leakage. The number of connections should be minimized, as any connection can be considered a potential leak point. U-shaped tubing can be implemented to eliminate unnecessary connections. Flange adaptors and extended male connectors can be used to reduce the number of threaded connections, as threaded connections pose a higher risk of leaking.
Instrumentation, such as flow meters, pressure gauges, and thermometers, should be considered early in project planning. Proper instrumentation can confirm process efficiency and can allow personnel to be proactive. For example, an increased temperature can indicate impeded flow or inefficient cooling. Appropriate instrumentation allows issues like this to be detected early to prevent mechanical seal damage or failure.
Gas Distribution Systems
Gas distribution systems are widely used in many petrochemical facilities and biotechnology facilities to deliver gas to laboratories, analyzers, or process equipment. Gas panels for distribution systems are the primary pressure control point and must reduce the pressure from a gas cylinder to deliver the gas to the point of use at the correct flow rate and pressure for a specific application.
Standardization of gas distribution systems and their associated subsystems, such as gas panels, can greatly simplify operation and maintenance procedures across a facility to reduce the risk of operator error and promote safe operations.
Pressure regulator selection plays heavily into gas routing characteristics and components selection for gas panels. Single-stage regulators typically show minimal droop with varying flow rates but experience a supply pressure effect. Dual-stage regulators typically yield minimal supply pressure effects but show a steeper slope in droop. Droop is the reduction of outlet pressure experienced by pressure-reducing regulators as the flow rate increases. So as the flow increases, the outlet pressure drops. It becomes a balance of forces.
Sampling Stations
Continuous and grab sampling stations are key to make informed decisions regarding the process and maintain quality control within a facility. Pressure, temperature, phase, and chemical composition of process fluid all affect sampling system design and materials of construction.
Routing within a sampling system is vital for obtaining representative samples. Dead legs can be a significant problem for sampling systems. If not properly managed, they can lead to misrepresentative samples or corrosion which may threaten piping integrity over time. Thus, dead legs should be minimized wherever possible in sampling systems and a proper purging mechanism should be implemented.
Similar to gas panels, standardization of sampling stations across a facility promotes ease of maintenance and can ensure that the sampling procedure is easily repeatable for facility personnel.
Look to Fluid Systems Experts for Optimal Routing
The design of industrial fluid systems’ routing can reduce costs and time spent during the maintenance phase of oil and gas and petrochemical facilities. Investing in quality prefabricated designs upfront not only saves time and money on field labour, but also provides a baseline for reliable, safe, and efficient pumping, gas distribution, and sampling operations.
With over 50 years of experience providing industrial fluid system solutions, Edmonton Valve & Fitting has extensive knowledge of solving local challenges in central and northern Alberta. Our local Field Advisors are readily available for consultations to analyze your design and process conditions and suggest solutions to help optimize industrial fluid systems’ routing. All of our fluid systems are locally fabricated and tested to ensure proper functionality and quality prior to delivery.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)