Share this
Vaporizing Regulators Help Maximize Analyzer Uptime
by Luke Wurban on Wed, Feb 12, 2020 @ 14:02 PM
Improvements to Swagelok's KEV Series mean better performance

Swagelok's improvements to its KEV Series Heated Regulators include better components and features that can prevent costly downtime. It has been designed to simplify assembly and maintenance in a way that is ergonomic and intuitive to help minimize the potential for operator errors, asset damage, and incorrect readings.
Turn up the heat
Suppose your process stream is liquid but you need a vaporized sample for analysis by a gas chromatograph. Likewise, you may need to apply heat in order to replace heat lost after a drop in pressure for gas systems, preventing condensation. In both cases, it's time to turn up the heat using a vaporizing regulator.
While it may sound simple — just heat the sample and analyze — an incorrectly designed system can result in incomplete vaporization, additional unwanted fractionation, and possibly long time delays. Here are a few challenges to be aware of, and how the Swagelok KEV Series of heated regulators deals with them.
Heat, but not too much
In general you need heat to vaporize a sample, but you don't want the heat to change the sample’s composition. You also want to avoid incomplete vaporization, fractionation, and excessive time delay. And the vaporizing equipment needs to remain reliable, even when there are changes in pressures along the flow path, changes in ambient conditions, or changes in operator inputs.
Different materials will put a different load on a vaporizing regulator. For example, it takes more energy to change the temperature of a fluid that's very cold, has a high density, or has a high flow rate.
If this thermal load drops dramatically (such as when an upstream valve is closed), there may be excess heat within the body, causing the thermal safety fuse to trip and cutting off all power to the heater element.
Similarly, if the load increases (such as when a flow control valve opens too far), the heater controller quickly delivers more power to the heater. This quick reaction can lead to a temperature overshoot, which likewise could trip a thermal safety fuse.
Swagelok's advantage
In the past year, Swagelok has made big improvements to its KEV Series Heated Regulator design to improve reliability and responsiveness by allowing for thermal feedback and adjustment to changing conditions.
The amount of power delivered to the KEV Series regulator is proportional to how far the temperature is from the regulator setpoint, the amount of time spent above or below the setpoint, and the rate of change of the temperature.
The KEV Series uses a Proportional Integral Derivative (PID) controller to manage the power level of the heater. The model was refined and tested by simulating its response under a variety of thermal load conditions. The simulation results were then correlated with actual data. The result is a well-tuned PID control loop that reacts quickly to changes in thermal load without overshooting or undershooting the target temperature.
Ambient temperature effects
It is common to install vaporizing regulators within heated enclosures. When designed correctly, they should run just fine. However, vaporizing regulators are often installed close to the enclosure heaters —in the worst case, directly above the heater. Since heat rises, the temperature surrounding the regulator will rise. That may work in steady-state conditions, but it will be difficult to shed any excess heat if the regulator must react to a change in flow or thermal load.
The KEV Series Regulator adapts to these challenging environmental conditions. An automatically re-settable, embedded thermal switch notifies the heater controller when overheating is imminent. The controller responds by interrupting power to the heater. Once the thermal switch resets, the controller automatically adjusts power output and resumes normal PID control. Learn more about our KEV Series Heated Regulator by downloading the one-page quicklook info sheet.
Operator Adjustment
Vaporizing regulators are not plug-and-play units. Analytical sample systems that include vaporizing regulators must be initially adjusted and maintained on a regular basis. Operators must know how to set proper power levels.
Fortunately you aren't left on your own with the KEV series. Our field engineers will properly size it and set it up using specialized software. Proper sizing of vaporizing regulators is a key to success. Every stream has a different composition, and these numbers are key ingredients to an efficient analytical system.
We're ready to help
The improved design of the Swagelok KEV Series Heated Regulator can react to changing thermal loads, can adjust power output to match system conditions, and can compensate for power levels. This keeps sample systems running well, maximizes your system’s effectiveness, and minimizes costly downtime. Click here to learn more about the regulators that we have available.
Edmonton Valve & Fitting is an expert on regulators, and we know how to advise and help. Put that combination to work for you by calling 780-437-0640 to ask about our KEV Series Heated Regulator, or send us a note through our website. Also ensure you're up to date with all Edmonton Valve & Fitting news and product launches by following us on LinkedIn.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)