Share this
Top Flow Assurance Challenges for SAGD Operations—And How to Prevent Them
by Tristian McCallion on Tue, Aug 10, 2021 @ 12:08 PM

The term “flow assurance” has expanded from its original use to describe flow problems in offshore oil and gas operations to encompass maintaining flow from one point to another for any type of oil and gas operation—for example, steam-assisted gravity drainage (SAGD) wells.
SAGD operations use flow assurance analysis to understand the composition and characteristics of the production fluid—a mixture of bitumen and water—and how it flows from the well to the surface to a processing plant. However, as SAGD wells age, the fluid characteristics of the production fluid change. It’s important to understand these changes to know how to adjust processes over the lifetime of the well.
Using good sampling practices with a well-designed system is the best way to ensure a thorough, up-to-date understanding of fluid characterization—which allows you to identify potential problems early in efforts to prevent them. In this post, we will look at some common flow assurance challenges in SAGD operations and how good sampling practices can work to prevent them.
Common Flow Assurance Challenges in SAGD Operations
SAGD operations rely on boilers to produce steam and pumps to move the product from place to place. Both pumps and boilers are critical failure points that can shut down operations if major problems occur.
Pumps
Plugged Seal: The high viscosity, solids-containing crude oil in SAGD wells makes plugs a common problem. Plugged seals can prevent the flush system from adequately flushing and lubricating the mechanical seal, which can ultimately lead to damage or failure.
Process Fluid Mixing with Buffer or Barrier Fluid: If high-viscosity process fluid leaks into the buffer/barrier fluid, it is very likely to plug the seal. This can overheat the mechanical seal, leading to leaking or failure. It is important to select a buffer/barrier fluid that resists the diffusion of process fluid.
Mechanical Seal Heat Checking: Heat checking in rotating equipment is a significant risk in SAGD operations because of the high temperatures and high-viscosity fluids. Heat checking happens when flow problems lead to insufficient seal lubrication or cooling.
Boilers
Scale and Corrosion: Clean water is essential to efficient and reliable boiler operation. Higher-quality steam leads to a higher recovery factor and lower steam-oil ratio (SOR). About 90% of SAGD water is treated and reused in the boiler, so it is necessary to sample and test the treated water regularly. Improperly treated water can leave scale or corrosion on boiler tubes, which can increase operating temperatures, decrease efficiency, and eventually cause failure.
Accurate Sampling Prevents Flow Assurance Problems Before They Occur
Understanding the composition of the process fluid is critical to ensure flow and maintain efficient and reliable SAGD operations. A simple and effective way to do this is with periodic grab sampling. Grab samples, along with proper instrumentation, provide insight into produced fluid’s viscosity, temperature, pressure, and water-to-oil ratio and how they change and affect flow over time. This allows you to be proactive with adjustments to the process to keep the system optimized.
Samples must be as representative of the process fluid as possible, so they must be fully mixed and cannot be contaminated during or after sampling. Ensure your samples are clean and representative by following these guidelines.
Use the Right Container: After collecting a sample, it is important to use a container that can maintain the sample at process conditions. Gases and volatile liquids require pressurized sample cylinders to prevent evaporation and fractionation. Bottles are an option only if the sample is an unpressurized, non-volatile, non-toxic liquid.
Avoid Contamination: Purge the line and container before sampling. Collect the sample with a smooth bore, not a corrugated hose. Analyze the sample as soon as possible to minimize the risk of contamination.
Avoid Phase Changes: Evaporation or condensation in the sampling line will alter the composition of the sample. Avoid phase changes by maintaining adequate pressure and temperature during collection. Use the P-T diagram of the fluid to understand the pressure and temperature needed to prevent phase changes, and never sample a fluid close to its phase change point.
Sample from the Right Location: Draw the sample from the middle third of the process line. The faster-moving fluid in the centre of the line is better mixed, while the slower-moving fluid near the wall is generally less representative of the process. Don’t sample from the bottom of the line where solids can collect.
Avoid Dead Legs: Dead legs are spaces in the system with no flow—like tees, pressure gauges, and temperature indicators—where solids and old fluid accumulate. Avoid drawing samples downstream of dead legs, and try to install these components downstream of the sampling station so they won’t affect sample integrity.
Look to Local Fluid Handling Experts for Grab Sampling Support
Edmonton Valve & Fitting is experienced with SAGD applications in Alberta and understands the flow assurance challenges of heavy crude oil. Our Field Advisors can perform a fluid systems evaluation to determine the best sampling system solution for your SAGD operations. Whether you need to repair or replace your current grab sampling system or you need a new one, our Field Advisors can help you understand your options.
Field Advisors at Edmonton Valve & Fitting can provide an onsite evaluation of your process to determine the best grab sampling solution. Our Field Advisors have ample experience with sampling systems for a wide range of SAGD applications and can make suggestions for improving SAGD efficiency.
About Tristian McCallion, Custom Solutions Manager, Edmonton Valve
Edmonton Valve has relied on McCallion for 26 years. His current title is Custom Solutions Manager. Earlier, he supervised our sales team. Before that, he managed sales throughout Edmonton and northeastern Alberta. For 12 years he also worked with Swagelok Energy Advisors across North America, training customers on steam fundamentals (TAP), testing steam traps, and conducting steam system audits.
Share this
- Fittings (82)
- Cost Savings (70)
- Valves (67)
- Fabrication (58)
- Services (40)
- Videos (33)
- Steam Systems (29)
- Training (27)
- Downloads (25)
- Resources (25)
- Tubing (24)
- Sampling (23)
- Field Advisors (18)
- Hoses (12)
- Oil & Gas (10)
- Regulators (9)
- Winterization (9)
- Gas Distribution (7)
- Hydrogen & Clean Energy (4)
- About Us (2)
- Measurement (2)
- July 2026 (2)
- February 2025 (1)
- November 2024 (1)
- October 2024 (2)
- August 2024 (1)
- July 2024 (1)
- June 2024 (4)
- April 2024 (4)
- March 2024 (2)
- January 2024 (3)
- December 2023 (2)
- November 2023 (3)
- October 2023 (2)
- September 2023 (3)
- August 2023 (3)
- July 2023 (3)
- June 2023 (2)
- May 2023 (4)
- April 2023 (2)
- March 2023 (2)
- February 2023 (3)
- January 2023 (2)
- December 2022 (1)
- November 2022 (1)
- October 2022 (2)
- September 2022 (5)
- August 2022 (3)
- July 2022 (6)
- June 2022 (4)
- May 2022 (3)
- April 2022 (1)
- March 2022 (2)
- February 2022 (3)
- January 2022 (4)
- December 2021 (4)
- November 2021 (6)
- October 2021 (3)
- September 2021 (5)
- August 2021 (9)
- July 2021 (5)
- June 2021 (7)
- May 2021 (7)
- April 2021 (4)
- March 2021 (3)
- February 2021 (3)
- January 2021 (2)
- December 2020 (3)
- November 2020 (3)
- October 2020 (2)
- September 2020 (3)
- August 2020 (3)
- July 2020 (3)
- June 2020 (3)
- May 2020 (3)
- April 2020 (2)
- March 2020 (3)
- February 2020 (3)
- January 2020 (3)
- December 2019 (2)
- November 2019 (3)
- October 2019 (3)
- September 2019 (2)
- August 2019 (3)
- July 2019 (2)
- June 2019 (2)
- May 2019 (3)
- April 2019 (3)
- March 2019 (3)
- February 2019 (2)
- January 2019 (3)
- December 2018 (2)
- November 2018 (2)
- October 2018 (4)
- September 2018 (2)
- August 2018 (3)
- July 2018 (3)
- June 2018 (2)
- May 2018 (4)
- April 2018 (2)
- March 2018 (3)
- February 2018 (3)
- January 2018 (4)
- December 2017 (1)
- November 2017 (4)
- October 2017 (4)
- September 2017 (4)
- August 2017 (5)
- July 2017 (3)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (5)
- February 2017 (4)
- January 2017 (4)
- December 2016 (3)
- November 2016 (3)
- October 2016 (4)
- September 2016 (3)
- August 2016 (4)
- July 2016 (2)
- June 2016 (2)
- May 2016 (2)
- April 2016 (4)
- March 2016 (2)
- February 2016 (3)
- January 2016 (4)
- December 2015 (4)
- November 2015 (4)
- October 2015 (5)
- September 2015 (2)
- August 2015 (4)
- July 2015 (5)
- June 2015 (2)
- May 2015 (3)
- April 2015 (5)
- March 2015 (3)
- February 2015 (4)
- January 2015 (3)
- December 2014 (4)
- November 2014 (4)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (4)
- January 2014 (4)
- December 2013 (3)
- November 2013 (4)
- October 2013 (5)
- September 2013 (4)
- August 2013 (5)
- July 2013 (4)
- June 2013 (3)
- May 2013 (4)
- April 2013 (5)
- March 2013 (2)
- February 2013 (3)
- January 2013 (5)
- December 2012 (2)
- November 2012 (3)
- October 2012 (5)
- September 2012 (3)
- August 2012 (4)
- July 2012 (4)
- June 2012 (1)